imx8mmevk : i2c register access is not working using md command in u-boot or memtool in userspace

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx8mmevk : i2c register access is not working using md command in u-boot or memtool in userspace

996件の閲覧回数
jagsgediya
Contributor II

When I try to read i2c controller register from u-boot shell using md command on imx8mmevk board it causes exception and resets the board, no variant of md command like md.b, md.w etc is working

u-boot=> md 0x30a20000
"Synchronous Abort" handler, esr 0x96000210
elr: 000000004029aea0 lr : 000000004029adf0 (reloc)
elr: 00000000bed8aea0 lr : 00000000bed8adf0
x0 : 0000000000000009 x1 : 00000000bcce5818
x2 : 00000000fffffffe x3 : 0000000000000020
x4 : 0000000000000000 x5 : 00000000bcce5810
x6 : 0000000000000030 x7 : 00000000bcce5760
x8 : 0000000000000010 x9 : 0000000000000008
x10: 00000000ffffffd8 x11: 0000000000000010
x12: 000000000001869f x13: 00000000bcce5a88
x14: 00000000bcce5b90 x15: 0000000000000021
x16: 00000000bed08a90 x17: 00000000000041a0
x18: 00000000bccefdb0 x19: 0000000000000004
x20: 0000000000000004 x21: 0000000000000004
x22: 0000000030a20000 x23: 00000000bcce5819
x24: 0000000000000000 x25: 00000000bcce57c8
x26: 00000000bedabbf0 x27: 0000000000000008
x28: 0000000000000004 x29: 00000000bcce5760

Code: 2a0403f3 17ffffcb 7100129f 54000181 (b94002c3)
Resetting CPU ..

 

Similarly when I try to access the I2C registers from linux user space using NXP's memtool, it causes board freeze,

root@imx8mm-lpddr4-evk:~# memtool I2C1.I2CR

Above command results into board hang.

What could be the possible reasons for above behavior?

iMX8MMINI iMX8M

0 件の賞賛
返信
1 返信

982件の閲覧回数
AldoG
NXP TechSupport
NXP TechSupport

Hello,

Have you tried using the raw address instead of the macro?
Also, please share the uboot and kernel version you're using.

Best regards,
Aldo.

0 件の賞賛
返信