imx8mmevk - 8mic-rpi-mx8: switch microphone geometry configuration

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

imx8mmevk - 8mic-rpi-mx8: switch microphone geometry configuration

1,562 次查看
Antares
Contributor II

Hello,

 

I am using a imx8mmevk with the 8mic-rpi-mx8. I built an image using Yocto (Zeus - 5.4.70) and flashed the imx8mmevk. I had to set "fdt_file" env in bootloader to "imx8mm-evk-8mic-revE.dtb" to be able to record data.

The microphone is now recognized by pulseaudio as "micfil" (alsa_input.platform-sound-micfil.stereo-fallback) - s16le - 2ch - 48000Hz.

 

From the quick start guide, the default configuration should be a 8 channels microphone. Do you have any idea why I get only 2 channels with pulseaudio ?

Secondly, I need to switch the geometry of the microphone to its 6 channels configuration. How could I do that ?

 

Best regards,

 

Loic

0 项奖励
回复
2 回复数

1,552 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Loic

 

one can try to change PDM configuration using Table 86. PDM Microphone controls,

sect.7.5 Audio Mixer (AUDMIX)   i.MX Linux Reference Manual​

https://source.codeaurora.org/external/imx/imx-test/tree/test/mxc_amix_test?h=lf-5.10.52_2.1.0

 

Best regards
igor

0 项奖励
回复

1,541 次查看
Antares
Contributor II

Hi Igor,

 

Thanks for the clue. I read this part of documentation and I can indeed change some PDM configuration.

But, I don't see anyway to update the mic array geometry in table 86. I can play with some parameters but it does not explain how to turn off some microphones.

 

Moreover, it says : "The captured audio format is 8-channels 32-bit wide linear
PCM audio data @ 48kHz". But pulseaudio, which get data from alsa, does not list any source supporting 8 channels capture. The micfil interface appears as above in pulse:

"alsa_input.platform-sound-micfil.stereo-fallback module-alsa-card.c s16le 2ch 44100Hz"

 

Best regards,

Loic

0 项奖励
回复