imx8mm verdin som board and carrier board downloading issues

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx8mm verdin som board and carrier board downloading issues

562件の閲覧回数
asif1206
Contributor I

Hello All

we have downloaded android 11.0.0.2.4 from NXP URL. we are able to build all the images.

 

Will flashing/ loading the image to board we are getting the following error.

./uuu_imx_android_flash_asif.sh -f imx8mm -a -e -t emmc -D /opt/android_build/out/target/product/evk_8mm/
This script is validated with uuu 1.4.139 version, it is recommended to align with this version.
dtbo is supported
dual slot is supported
dynamic parttition is supported
vendor_boot parttition is supported
asif 3-1-2022-->1
asif 3-1-2022-->2
u-boot-imx8mm-ddr4.imx
asif 3-1-2022-->2a
asif 3-1-2022-->3
generate lines to flash u-boot-imx8mm-ddr4.imx to the partition of bootloader0
generate lines to flash partition-table-14GB.img to the partition of gpt
generate lines to flash dtbo-imx8mm.img to the partition of dtbo_a
generate lines to flash boot.img to the partition of boot_a
generate lines to flash vendor_boot.img to the partition of vendor_boot_a
generate lines to flash vbmeta-imx8mm.img to the partition of vbmeta_a
generate lines to flash super.img to the partition of super
uuu script generated, start to invoke uuu with the generated uuu script
uuu (Universal Update Utility) for nxp imx chips -- libuuu_1.4.139-0-g1a8f760

Success 0 Failure 1


3:3 3/20 [ ] FB: ucmd mmcdev

Thanks  & Regards

Asif

 

 

0 件の賞賛
返信
1 返信

556件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Asif

 

>we have downloaded android 11.0.0.2.4 from NXP URL. we are able to build all the images.

 

this release was developed for NXP reference boards, like i.MX8M Mini EVK, while

"imx8mm verdin som board" is different third party board:

https://developer.toradex.com/products/verdin-imx8m-mini

So it is necessary to perform changes to NXP sources for that different board, for

example uboot ddr4 timings e.t.c.

https://source.codeaurora.org/external/imx/uboot-imx/tree/board/freescale/imx8mm_evk/ddr4_timing.c?h...

 

Best regards
igor

0 件の賞賛
返信