Hello All
we have downloaded android 11.0.0.2.4 from NXP URL. we are able to build all the images.
Will flashing/ loading the image to board we are getting the following error.
./uuu_imx_android_flash_asif.sh -f imx8mm -a -e -t emmc -D /opt/android_build/out/target/product/evk_8mm/
This script is validated with uuu 1.4.139 version, it is recommended to align with this version.
dtbo is supported
dual slot is supported
dynamic parttition is supported
vendor_boot parttition is supported
asif 3-1-2022-->1
asif 3-1-2022-->2
u-boot-imx8mm-ddr4.imx
asif 3-1-2022-->2a
asif 3-1-2022-->3
generate lines to flash u-boot-imx8mm-ddr4.imx to the partition of bootloader0
generate lines to flash partition-table-14GB.img to the partition of gpt
generate lines to flash dtbo-imx8mm.img to the partition of dtbo_a
generate lines to flash boot.img to the partition of boot_a
generate lines to flash vendor_boot.img to the partition of vendor_boot_a
generate lines to flash vbmeta-imx8mm.img to the partition of vbmeta_a
generate lines to flash super.img to the partition of super
uuu script generated, start to invoke uuu with the generated uuu script
uuu (Universal Update Utility) for nxp imx chips -- libuuu_1.4.139-0-g1a8f760
Success 0 Failure 1
3:3 3/20 [ ] FB: ucmd mmcdev
Thanks & Regards
Asif
Hi Asif
>we have downloaded android 11.0.0.2.4 from NXP URL. we are able to build all the images.
this release was developed for NXP reference boards, like i.MX8M Mini EVK, while
"imx8mm verdin som board" is different third party board:
https://developer.toradex.com/products/verdin-imx8m-mini
So it is necessary to perform changes to NXP sources for that different board, for
example uboot ddr4 timings e.t.c.
Best regards
igor