[imx8mm] tinycompress test tool not working on Yocto image

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

[imx8mm] tinycompress test tool not working on Yocto image

跳至解决方案
260 次查看
krzysztof-buczak-red
Contributor I

Hello,

I have imx8mm EVK platform with image:

LF_v6.6.52-2.2.1_images_IMX8MMEVK/imx-image-full-imx8mmevk.wic

flashed on it. When I was trying to use a test tool cplay that is shipped with package tinycompress, I encountered following error:

root@imx8mmevk:~# cplay test.mp3
Unable to open Compress device 0:0
ERR: cannot open device '/dev/snd/comprC0D0': No such file or directory

In fact, I don't see any comprCxDy devices under /dev/snd/, so modifying the tool call with flags has no effect as it always ends up looking for compress devices. Could you help me determine if it's possible to make this example work? I suppose tinycompress is installed mostly as a gstreamer dependency, but I was wondering if it can work standalone, e.g. via mentioned cplay tool example.

标签 (1)
1 解答
223 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

Cplay is not the default in yocto bsp, you should try  aplay -D plughw:0,0 your_sound.wav

 

Regards

在原帖中查看解决方案

0 项奖励
回复
1 回复
224 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

Cplay is not the default in yocto bsp, you should try  aplay -D plughw:0,0 your_sound.wav

 

Regards

0 项奖励
回复