imx8mm sai1 can't open

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx8mm sai1 can't open

1,114 Views
14766419
Contributor I

HI:

I'm using i.mx8mm to develop audio, and I'm using SAI1. Why is this problem all the time?

root@okmx8mm:~# aplay -Dhw:1,0 /home/forlinx/audio/w1.wav
[ 72.078013] fsl-sai 30010000.sai: ASoC: can't open platform 30010000.sai: -6

root@okmx8mm:~# aplay -l
**** List of PLAYBACK Hardware Devices ****
card 0: wm8960audio [wm8960-audio], device 0: HiFi wm8960-hifi-0 []
Subdevices: 1/1
Subdevice #0: subdevice #0
card 1: imxaudioadau145 [imx-audio-adau1452], device 0: adau1452 adau1452-tdm-0 []
Subdevices: 1/1
Subdevice #0: subdevice #0

Thanks!

Labels (1)
0 Kudos
Reply
1 Reply

998 Views
igorpadykov
NXP Employee
NXP Employee

Hi chen

one can look at i.mx8mm dts file

fsl-imx8mm-evk.dts\freescale\dts\boot\arm64\arch - linux-imx - i.MX Linux kernel 

and check codecs connected to sai1:  ak4458, ak4497.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply