imx8mm-lpddr4-evk yocto build stuck at 99%

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

imx8mm-lpddr4-evk yocto build stuck at 99%

852 次查看
vignesh-baskaran
Contributor III

Hi,

We were trying to build yocto build for imx8mm-lpddr4-evk.

$ DISTRO=fsl-imx-wayland MACHINE=imx8mm-lpddr4-evk source imx-setup-release.sh -b <build folder>

$ bitbake imx-image-core

This is fresh build, we didn't made any changes to it.

Currently 1 running tasks (6175 of 6208) 99% |###################################################################################################################### |
0: u-boot-imx-2022.04-r0 do_compile - 2h42m3s (pid 12465)

 

it was stuck like this.

Screenshot from 2023-02-24 18-32-47.png

Can you let us know any solution to this one?

 

Thanks

 

 

 

 

0 项奖励
回复
1 回复

826 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

Is probably you are not in the rigth image or you have a bad ram to to run:

core-image-minmal

and https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX-8M-Family-DDR-Tool-Release/ta-p/110...

Regards

 

 

 

 

 

 

0 项奖励
回复