imx8mm gpio error _gpiod_direction_output_raw tried to set a GPIO tied to an IRQ as output

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx8mm gpio error _gpiod_direction_output_raw tried to set a GPIO tied to an IRQ as output

Jump to solution
4,036 Views
jianfeichang
Contributor IV

imx8mm linux kernel 4.14.98 ,kernel-4.14.98/drivers/hwmon/sht15.c

log error:

insmod sht15.ko
[ 425.787145] gpio-82 (SHT15 data): _gpiod_direction_output_raw: tried to set a GPIO tied to an IRQ as output
[ 425.796987] sht15: probe of p8-ports failed with error -5

dts:

231 pinctrl_p8_ports: p8_ports_grp {
232      fsl,pins = <
233           MX8MM_IOMUXC_NAND_WE_B_GPIO3_IO17 0x19
234           MX8MM_IOMUXC_NAND_WP_B_GPIO3_IO18 0x19
235       >;
236 };

sht15.c:

devm_request_irq(&pdev->dev, gpio_to_irq(data->pdata->gpio_data),

disable_irq_nosync(gpio_to_irq(data->pdata->gpio_data));

gpio_direction_output(data->pdata->gpio_data, 1);

dts change MX8MM_IOMUXC_NAND_WP_B_GPIO3_IO18 0x80000000 is error,imx6 3.14.28 is ok,imx6 4.9.88 is error。

The following is the Chinese translation:

--------------------------------------------------------------------------------

imx8mm 内核4.14.98Linux系统,sht15.c文件里,把GPIO设置成中断,然后失能中断,然后切换到GPIO输出,提示不行,把设备树配置成0x80000000也不行,imx6 3.14.28内核可以,imx6的4.9.88不行。

0 Kudos
Reply
1 Solution
3,997 Views
jianfeichang
Contributor IV

Hi igorpadykov

Thank you for your reply.

Can I change the imX8 pins? I don't think the kernel will be modified, it's just upgraded to solve some configuration problems that don't make sense。

View solution in original post

0 Kudos
Reply
2 Replies
4,017 Views
igorpadykov
NXP Employee
NXP Employee

Hi jianfeichang

 

seems this feature is not supported on last kernels as described on other forums, like:

https://github.com/raspberrypi/linux/issues/808

One can post issue on kernel mail list:

http://vger.kernel.org/vger-lists.html

 

Best regards
igor

0 Kudos
Reply
3,998 Views
jianfeichang
Contributor IV

Hi igorpadykov

Thank you for your reply.

Can I change the imX8 pins? I don't think the kernel will be modified, it's just upgraded to solve some configuration problems that don't make sense。

0 Kudos
Reply