ar6k_wlan: probe of mmc0:0001:1 failed with error -1.
We are using i.MX 8MM EVK with the latest Android 10.0.0_2.5.0 and Wi-Fi is not working as it is also using "QCA9377".
Any update or migration guide how to use the existing WiFi module for wireless connection?
Hello,
Yes you're correct for this release the i.MX 8M Mini EVK LPDDR4 board, BT function is supported as is (1PJ QCA9377).
Wi-Fi function for the other side is supported with the Wi-Fi expansion card (NXP 88W8987) plugged to the SD card slot.
Andorid Q10.0.0_1.0.0 still support both BT and Wi-Fi using the 1PJ QCA9377.
Unfortunately we have no plans to support QCA9377 in future releases.
Best regards,
Aldo.