imx8mm can not shutdown after upgrade to lf-5.10.72-2.2.2

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx8mm can not shutdown after upgrade to lf-5.10.72-2.2.2

289件の閲覧回数
ChicLee
Contributor I

Hi, 

before upgrade, our device(hardknott-5.10.72-2.2.1) can normal shutdown after "poweroff" command.

but upgrade to lf-5.10.72-2.2.2, our device can not normal shutdown after "poweroff" command.

I found the commit from imx-atf and it makes the problem.

I want to know what is the next I should do? check schematic? or check the kernel source?

Thanks

 

ラベル(1)
0 件の賞賛
返信
0 返答(返信)