imx8mm SAI1 录音失败

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

imx8mm SAI1 录音失败

467 次查看
yzg
Contributor I

你好:

我在imx8mm使用sai1录音的时候遇到了问题,现在sai1可以正常播放音频,但是录音的时候会出现下面的情况,我测量了时钟都正确的 .

Recording WAVE 'stdin' : Signed 16 bit Little Endian, Rate 48000 Hz, Stereo
RIFF$▒WAVEfmt ▒▒▒data▒overrun!!! (at least 1008.666 ms long)
overrun!!! (at least 1001.840 ms long)
overrun!!! (at least 1002.542 ms long)
overrun!!! (at least 1009.403 ms long)

0 项奖励
回复
1 回复

446 次查看
Harvey021
NXP TechSupport
NXP TechSupport

Hello yzg.

What is the BSP with which your MM is working please?  and also please share us your commands being executed while recording. It would be better to share codes that if you modify.

I here share a link, Add audio record driver in i.MX8MQ&MM.pdf, which includes a document for how to add drivers.

Add audio record driver in i.MX8MQ/8MM - NXP Community

 

Best regards

Harvey

0 项奖励
回复