imx8mm - GPT clock source

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx8mm - GPT clock source

3,833件の閲覧回数
nirgeller
Contributor I

Hi There,

I'm working on a imx8mm evaluation board, running BSP 5.4-zeus, BB_VERSION = "1.44.0", linux kernel 5.4.47.

I'm trying to set clock source to the GPT.

According to "i.MX 8M Mini Applications Processor Reference Manual", page 280, Table 5-1, the maximum clock frequency that can be used is 100MHz.

nirgeller_0-1614105283868.png

 

According to page 3855, 12.1.5.1, GPT Control Register, the clock source can be determined by setting bits 8-6 during the setup procedure of the GPT. 

nirgeller_1-1614105412796.png

By editing the GPT driver, drivers/clocksource/timer-imx-gpt.c I tried all the variants, but the maximum clock frequency I got is 24MHz.

 

Please help me to configure that clock source to get at least 66MHz.

 

Thanks,

 

Nir.

0 件の賞賛
返信
4 返答(返信)

3,811件の閲覧回数
nirgeller
Contributor I

Hi Igor,

Thanks for your reply.

It looks like the clock driver, drivers/clk/imx/clk-imx8mm.c, defines the available clock sources for the GPT module in line 301:

301 static const char *imx8mm_gpt1_sels[] = {"osc_24m", "sys_pll2_100m", "sys_pll1_400m", "sys_pll1_40m",
302 "video_pll1_out", "sys_pll1_80m", "audio_pll1_out", "clk_ext1" };

This definition complies perfectly with Table 5-1.

However, the clock source is determined by bits 6-8 in the GPT control register, 12.1.5.1

How exactly are these 3 bits mapped to the structure imx8mm_gpt1_sels[]?

How can I figure out what is the frequency of "High Frequency Reference Clock (ipg_clk_highfreq)", or "Peripheral Clock (ipg_clk)"?

As I stated, any combination of bits I'm trying yields a maximum frequency of 24MHz. (I'm setting the prescaler to 1).

Can you please direct me how to set sys_pll2_100m as the clock source instead of osc_24m?

Thanks a lot,

Nir.

0 件の賞賛
返信

3,780件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Nir

 

one can try to debug it using AN4553 Using Open Source Debugging Tools for Linux on i.MX Processors
https://www.nxp.com/docs/en/application-note/AN4553.pdf

Also I sent additional patch by mail, however for complete solution suggest to proceed with help of

https://contact.nxp.com/new-prof-svcs-sw-tech

 

Best regards
igor

0 件の賞賛
返信

3,792件の閲覧回数
nirgeller
Contributor I

Hi Igor,

Thanks for your reply.

It looks like the clock driver, drivers/clk/imx/clk-imx8mm.c, defines the available clock sources for the GPT module in line 301:

301 static const char *imx8mm_gpt1_sels[] = {"osc_24m", "sys_pll2_100m", "sys_pll1_400m", "sys_pll1_40m",
302 "video_pll1_out", "sys_pll1_80m", "audio_pll1_out", "clk_ext1" };

This definition complies perfectly with Table 5-1.

However, the clock source is determined by bits 6-8 in the GPT control register, 12.1.5.1

How exactly are these 3 bits mapped to the structure imx8mm_gpt1_sels[]?

How can I figure out what is the frequency of "High Frequency Reference Clock (ipg_clk_highfreq)", or "Peripheral Clock (ipg_clk)"?

As I stated, any combination of bits I'm trying yields a maximum frequency of 24MHz. (I'm setting the prescaler to 1).

Can you please direct me how to set sys_pll2_100m as the clock source instead of osc_24m?

Thanks a lot,

Nir.

0 件の賞賛
返信