imx8mm 4G ddr stress test fail

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx8mm 4G ddr stress test fail

ソリューションへジャンプ
855件の閲覧回数
jiangyaqiang
Contributor IV

Hi anyone:

    I got a problem with "ddr stress test" for 4G ddr in imx8mini, using mscale_ddr_tool _v3.20.

    It end up show 2GB only ,and calibration fail:

    But there is no problem with imx8mq with the same IC.

    And the board(imx8mm) could boot up with board/freescale/imx8mm_evk/lpddr4_timing_4g.c 

 

here are the log of imx8mm and imx8mq:

imx8mm:

jiangyaqiang_0-1717498513723.jpeg

imx8mq:

jiangyaqiang_1-1717498675310.jpeg

Any help is appreciate.

ラベル(1)
0 件の賞賛
返信
1 解決策
600件の閲覧回数
jiangyaqiang
Contributor IV

it's config issue, the "Density per channel per chip select (Gb)1:" is wrong.

Here is the correct one/

元の投稿で解決策を見る

0 件の賞賛
返信
10 返答(返信)
601件の閲覧回数
jiangyaqiang
Contributor IV

it's config issue, the "Density per channel per chip select (Gb)1:" is wrong.

Here is the correct one/

0 件の賞賛
返信
841件の閲覧回数
JorgeCas
NXP TechSupport
NXP TechSupport

Hello,

 

I suggest you try with our latest RPA version available.

 

Could you please share the logs when calibration fails?

 

Bets regards.

0 件の賞賛
返信
819件の閲覧回数
jiangyaqiang
Contributor IV

Hi JorqeCas: 

 

Thanks for reply. 

I have tried the latest RPA, the result is same.

It could not recognize as 2GB only, and calibration fail .

Attached log and RPA.

0 件の賞賛
返信
775件の閲覧回数
JorgeCas
NXP TechSupport
NXP TechSupport

Hello,

I do not see issues on your RPA configuration.

For that error is recommended check the layout firstly.

Also you can lower the DDR speed to try.

Could you please try with DDR tool of Config Tools for i.MX?

Best regards.

 

0 件の賞賛
返信
765件の閲覧回数
jiangyaqiang
Contributor IV

Hi JorgeCas:

 

 Thanks.

But could you share you RPA and stress test log ?

I'm fail at 4GB, but no problem with 2GB/3GB.

BTW, my ddr row=16 for 4GB, it's the same with 2GB/3GB.

It fail , no because the board is not stable, but the stress tool could not recognize it as 4GB, but 2GB instead .

 

And the layout is no problem. The board  could bootup good .

And the board test stable with 2GB/3GB lpddr4. 

 

0 件の賞賛
返信
587件の閲覧回数
Ajesh_Ametek1
Contributor I

MT53E1G32D2FW-046 WT:B has 17 row address lines. As per your RPA sheet, 'Number of ROW Addresses' is set to 16. That is why may be you are able to see 2GB.

Ajesh_Ametek1_0-1718278336512.png

 

 

0 件の賞賛
返信
557件の閲覧回数
jiangyaqiang
Contributor IV

HI Ajech_Ametak1:

 

You datasheet should be MT53E1G32D2FW-046 WT:C , not MT53E1G32D2FW-046 WT:B, 

for "B" one 16 row, or "C"  row is 17.

0 件の賞賛
返信
538件の閲覧回数
Ajesh_Ametek1
Contributor I

Hi @jiangyaqiang 

Yes... I was referring to MT53E1G32D2FW-046 WT:C datasheet... 

0 件の賞賛
返信
759件の閲覧回数
JorgeCas
NXP TechSupport
NXP TechSupport

Hello,

I used the default .ds file provided with the tool for i.MX8MM EVK (mx8mm_micron_lpddr4_2gb_2d_1500m_200m_50m_32bit_1cs_RPAv18.ds).

Right now, I do not have access to the board until next Monday I will share it with you if you need it but, it passed the test with 2GB.

Is your board able to boot with 4GB and work as expected?

Did you try with Config Tools for i.MX?

Best regards.

0 件の賞賛
返信
748件の閲覧回数
jiangyaqiang
Contributor IV

Hi JorgeCas:

 

Yes , my board works with 4GB lpddr4_timing_4g.c. But I don't know it stable or not , event it not crash for hours. I do need to generate the lpddr4_timing_4g.c using my config.

If you test on board, it'better use 4GB one.

I have tested with "Config Tools for i.MX" version 15.1 . But the result is not acceptable , no matter how I config it , it will pass the test. For example , the following config(8GB) will pass the test too. And there is no "ODT" config for imx8mm imx8mp, but the document says it has.

jiangyaqiang_0-1717723603056.png

 

 

0 件の賞賛
返信