imx8mm作为I2S从设备,codec wm8960为主设备,能播放,不能录音

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx8mm作为I2S从设备,codec wm8960为主设备,能播放,不能录音

863 Views
1269813285
Contributor I

cpu芯片是imx8mm,codec芯片是wm8960,android版本是nxp_imx-p9.0.0_2.2.0,cpu为从,codec芯片为主设备,能够播放音乐,不能录音。

1. 设备树配置如下:

 

 

sound {
compatible = "fsl,imx6ul-evk-wm8960",
"fsl,imx-audio-wm8960";
model = "wm8960-audio";
cpu-dai = <&sai3>;
audio-codec = <&codec>;
codec-master;
gpr = <&gpr 4 0x100000 0x100000>;
hp-det = <2 0>;
hp-det-gpios = <&gpio4 0 0>;
mic-det-gpios = <&gpio4 0 0>;
audio-routing =
			"Headphone Jack", "HP_L",
			"Headphone Jack", "HP_R",
			"Ext Spk", "SPK_LP",
			"Ext Spk", "SPK_LN",
			"Ext Spk", "SPK_RP",
			"Ext Spk", "SPK_RN",
			"LINPUT1", "Main MIC",
			"LINPUT2", "Main MIC",
			"RINPUT1", "Hp MIC",
			"RINPUT2", "Hp MIC",
			"Mic Jack", "MICB",
			"Main MIC", "MICB",
			"CPU-Playback", "ASRC-Playback",
			"Playback", "CPU-Playback",
			"ASRC-Capture", "CPU-Capture",
			"CPU-Capture", "Capture";
	};

};
codec: wm8960@1a {
		compatible = "wlf,wm8960";
		reg = <0x1a>;
		clocks = <&clk IMX8MM_CLK_SAI3_ROOT>;
		clock-names = "mclk";
		wlf,shared-lrclk;
};
&sai3 {
	pinctrl-names = "default";
	pinctrl-0 = <&pinctrl_sai3>;
	assigned-clocks = <&clk IMX8MM_CLK_SAI3>;
	assigned-clock-parents = <&clk IMX8MM_AUDIO_PLL1_OUT>;
	assigned-clock-rates = <24576000>;
	status = "okay";
};
pinctrl_sai3: sai3grp {
			fsl,pins = <
				MX8MM_IOMUXC_SAI3_RXFS_SAI3_RX_SYNC     0xd6 
				MX8MM_IOMUXC_SAI3_TXFS_SAI3_TX_SYNC     0xd6
				MX8MM_IOMUXC_SAI3_TXC_SAI3_TX_BCLK      0xd6
				MX8MM_IOMUXC_SAI3_MCLK_SAI3_MCLK        0xd6
				MX8MM_IOMUXC_SAI3_TXD_SAI3_TX_DATA0     0xd6
				MX8MM_IOMUXC_SAI3_RXD_SAI5_RX_DATA0     0xd6
			>;
		};

pinctrl_sai3_hp_det_b: sai3_hp_det_grp {
			fsl,pins = <
				MX8MM_IOMUXC_SAI1_RXFS_GPIO4_IO0        0x16
			>;
		};

 

 

2. 没有修改imx-wm8960.c、wm8960.c、fsl_sai.c的代码。

3. LINPUT1作为main mic的输入端。 

4. 录音时寄存器值如下:

 

 

[  127.991755] reg=0x000 val=0x1bc
[  127.995640] reg=0x001 val=0x1bc
[  127.998813] reg=0x002 val=0x178
[  128.002111] reg=0x003 val=0x178
[  128.005476] reg=0x004 val=0x121
[  128.009389] reg=0x005 val=0x008
[  128.012584] reg=0x006 val=0x000
[  128.015766] reg=0x007 val=0x042
[  128.018912] reg=0x008 val=0x1cd
[  128.022127] reg=0x009 val=0x040
[  128.025343] reg=0x00a val=0x1e6
[  128.028520] reg=0x00b val=0x1e6
[  128.031674] reg=0x00c val=0x1e6
[  128.034816] reg=0x00d val=0x1e6
[  128.037999] reg=0x00e val=0x1e6
[  128.041164] reg=0x00f val=0x1e6
[  128.044339] reg=0x010 val=0x000
[  128.047533] reg=0x011 val=0x1fb
[  128.050686] reg=0x012 val=0x100
[  128.053868] reg=0x013 val=0x032
[  128.057045] reg=0x014 val=0x000
[  128.060202] reg=0x015 val=0x1e6
[  128.063355] reg=0x016 val=0x1e6
[  128.066497] reg=0x017 val=0x1c3
[  128.069737] reg=0x018 val=0x044
[  128.072934] reg=0x019 val=0x0ee
[  128.076127] reg=0x01a val=0x001
[  128.079293] reg=0x01b val=0x000
[  128.082501] reg=0x01c val=0x008
[  128.085673] reg=0x01d val=0x000
[  128.088827] reg=0x01e val=0x000
[  128.092079] reg=0x01f val=0x000
[  128.095251] reg=0x020 val=0x108
[  128.098393] reg=0x021 val=0x100
[  128.101576] reg=0x022 val=0x150
[  128.104745] reg=0x023 val=0x150
[  128.107976] reg=0x024 val=0x150
[  128.111148] reg=0x025 val=0x150
[  128.114291] reg=0x026 val=0x000
[  128.117468] reg=0x027 val=0x000
[  128.120622] reg=0x028 val=0x178
[  128.123780] reg=0x029 val=0x178
[  128.126922] reg=0x02a val=0x040
[  128.130141] reg=0x02b val=0x000
[  128.133305] reg=0x02c val=0x000
[  128.136475] reg=0x02d val=0x050
[  128.139654] reg=0x02e val=0x050
[  128.142804] reg=0x02f val=0x030
[  128.145989] reg=0x030 val=0x03a
[  128.149167] reg=0x031 val=0x037
[  128.152342] reg=0x032 val=0x037
[  128.155505] reg=0x033 val=0x080
[  128.158646] reg=0x034 val=0x027
[  128.161861] reg=0x035 val=0x059
[  128.165138] reg=0x036 val=0x099
[  128.168328] reg=0x037 val=0x09a

 

 

5. 通过示波器测量,当录音时,LINPUT1有模拟信号的输入,并且MCLK为24.576MHZ,BCLK为1.412MHZ,ADCLRC为44.1KHZ。

6.通过tinycap test.wav -T 50录音,没有报错,但是播放test.wav时却没有声音,

   Capturing sample: 2 ch, 44100 hz, 16 bit

7. 看kernel log,没有报错。

Labels (1)
0 Kudos
1 Reply

830 Views
xcyhere
Contributor I

你好:

    我也遇到同样的问题了,请问你后来解决了吗?怎么解决的呢?

0 Kudos