Thanks for reply,
we have checked as you suggested but facing same issue.
we have used below procedure for your method.
Here we have used linux version is 5.10.35 and imx8m mini evk board
1.we have disabled I2C3 in imx8mm-evk-rpmsg.dts file and complied
2. copied imx8mm-evk.dtb file into the boot partition
3. then M4 core booted and then A53 core booted with linux after this stage I2C peripheral under M4 core stops working
we have noticed that under the memory map A53 and M4 shares same memory for I2c and some other peripheral. And the APIS3 memory region is mention under the DTS driver code under linux. May be this is the reason for the issue.
Would like to if there any solution to over come this and give privilage to I2c under M4
also we have tried another method i.e with linux 5.10.35 prebuild demo image, for this also used same above procedure but still facing same issue "M4 core stops working after booting A53 core with linux version 5.10.35"
we stuck here Please suggest.
Thanks in Advance.