imx8m plus SD boot mode without changing BOOT_MODE[3:0] config

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

imx8m plus SD boot mode without changing BOOT_MODE[3:0] config

406 次查看
EJSHY
Contributor I

Hi NXP Team,

By default our system with MIMX8ML8 Is in MMC boot mode as BOOT_MODE[3:0] is configured to 0010 by HW strapping. 

Is there any way to put the IMX8ML plus to SD boot mode without changing the  BOOT_MODE[3:0] pins? Any fallback options if MMC doesn't have a proper image?

0 项奖励
回复
2 回复数

345 次查看
opedis
Contributor III

If the hardware design is correct, the SD/MMC manufacture mode will be working.

 

2024-02-22_084533.png

0 项奖励
回复

393 次查看
Chavira
NXP TechSupport
NXP TechSupport

Hi @EJSHY!
Thank you for contacting NXP Support!

I think it is possible, but we don't have examples or documentation about that.

You have to change the bootflow command on your board to determine the source that you want to boot.

Please check the official documentation for that.

https://docs.u-boot.org/en/latest/usage/cmd/bootflow.html

Sorry for the mistake!

Best Regards!

Chavira

0 项奖励
回复