imx8m nano can't get non-image data of mipi camera

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

imx8m nano can't get non-image data of mipi camera

跳至解决方案
1,150 次查看
link
Contributor III

Hi all:

      We use IMX8M Nano to adapt a MIPI camera. The output resolution of the camera is 1280*483. The Data type of MIPI packets in the first 480 lines is 0x2C, and that of MIPI packets in the last 3 lines is 0x12.

link_1-1631861701807.png

 

      The data we got from V4L2 was normal for the first 480 rows and '0' for the last three.Through the oscilloscope, we can confirm that the sensor output is normal.

link_1-1631858572331.png

     In the <i.MX 8M Nano Applications Processor Reference Manual>, the packets with Data type 0x10 and 0x11 are ignored.

link_0-1631858409629.png

    In the interrupt function we add log to confirm that the interrupt will only be triggered at Frame Start and Frame End. 

link_2-1631858947530.png

      I want to know whether the mipi packets data of 0x12 type is also ignored, and how to solve this problem?

 

Thanks & Best Regards,

link

标记 (1)
0 项奖励
回复
1 解答
1,137 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Yanlin

 

in general, hardware have the capability to receive packets data of 0x12 type,

but there is no software driver to support it. For help may be suggested to proceed with

https://contact.nxp.com/new-prof-svcs-sw-tech

 

Best regards
igor

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,138 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Yanlin

 

in general, hardware have the capability to receive packets data of 0x12 type,

but there is no software driver to support it. For help may be suggested to proceed with

https://contact.nxp.com/new-prof-svcs-sw-tech

 

Best regards
igor

0 项奖励
回复