imx8m mini mipi dsi

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx8m mini mipi dsi

1,421件の閲覧回数
story
Contributor II

hi,

I am using the mipi dsi interface of the imx8m mini, configured with the relevant dts, but did not detect the clk (DSI_CKP, DSI_CKN) signals of mipi dsi, DSI_DN0, DSI_DP0, DSI_DN1, DSI_DP1, DSI_DN2, DSI_DP2, DSI_DN3, DSI_DP3, DSI_DN4, Signals such as DSI_DP4 can measure waveforms, which may be the problem there?

ラベル(1)
0 件の賞賛
返信
1 返信

1,128件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi 扬 杨 

one can try Demo Image with i.MX8M Mini EVK

Linux Binary Demo Files - i.MX 8MMini EVK

More linux and android documentation can be found on

i.MX Software | NXP 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信