imx8m mini mipi dsi

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx8m mini mipi dsi

830 Views
story
Contributor II

hi,

I am using the mipi dsi interface of the imx8m mini, configured with the relevant dts, but did not detect the clk (DSI_CKP, DSI_CKN) signals of mipi dsi, DSI_DN0, DSI_DP0, DSI_DN1, DSI_DP1, DSI_DN2, DSI_DP2, DSI_DN3, DSI_DP3, DSI_DN4, Signals such as DSI_DP4 can measure waveforms, which may be the problem there?

Labels (1)
0 Kudos
1 Reply

537 Views
igorpadykov
NXP Employee
NXP Employee

Hi 扬 杨 

one can try Demo Image with i.MX8M Mini EVK

Linux Binary Demo Files - i.MX 8MMini EVK

More linux and android documentation can be found on

i.MX Software | NXP 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos