Hello,
I want to figure out how imx8m power management is done in Linux and cores are put into low power:
Q1- As I guessed, low power mode relates to power and clock. Is there any things except them?
Q2- Which Linux source files implement the reference manual stuffs relating to power and clock?
Q3- Is there any other document except reference manual about imx8m low power mode?
Thanks in advance
解決済! 解決策の投稿を見る。
also one can look at AN12225 How to Reduce SoC Power when Running M4 with A53 on i.MX8M
AN12195 Implement Low-Power Audio on i.MX8M
Best regards
igor
Hi igor,
The document describes some benchmarks. My question is about the low power functionality in i.MX8M.
Q1- How does the power management and clock system work at both sides Hardware and Linux?
Q2- Is there any other document except reference manual about these topics?
Thanks
also one can look at AN12225 How to Reduce SoC Power when Running M4 with A53 on i.MX8M
AN12195 Implement Low-Power Audio on i.MX8M
Best regards
igor
Hi igor,
My ultimate goal is to run a program on Cortex-M4 (CM4) to control a peripheral (e.g. GPIO, UART, CAN or etc) when Cortex-A (CA) cores are in sleep (i.e. echo mem > /sys/power/state).
The current implementation puts CM4 in sleep when Linux goes into sleep. As I searched the kernel source code, there are two important files: (These are just my guesses)
1- psci.c: is used to manage CA cores, e.g. put them into sleep
2- gpc-psci.c: is used to manage imx8 power domains, e.g. to turn off power of domain and put that domain into sleep
Q1- Are the power management operations (e.g. putting CA and CM4 into sleep) implemented in Linux source code (psci.c and gpc-psci.c) or in ATF (gpc.c)? I can't realize Linux and ATF relationship in handling power management.
Q2- I guess CA core0 is always ON and not put into sleep even if I use "echo mem > /sys/power/state". Is that right?
Q3- Are there any documents about imx8mq power domains except the reference manual?
Hi asghar
> My ultimate goal is to run a program on Cortex-M4 (CM4) to control a peripheral
>(e.g. GPIO, UART, CAN or etc) when Cortex-A (CA) cores are in sleep
>(i.e. echo mem > /sys/power/state).
such use case (example with audio) is provided in AN12195 Implement Low-Power Audio on i.MX8M
>Are there any documents about imx8mq power domains except the reference manual?
not, sorry.
Best regards
igor
Hi igor,
Thanks for your help.
what about this question:
Q2- I guess CA core0 is always ON and not put into sleep even if I use "echo mem > /sys/power/state". Is that right?
Hi asghar
> I guess CA core0 is always ON and not put into sleep even
>if I use "echo mem > /sys/power/state". Is that right?
not, sorry.
Best regards
igor
Hi Asghar
for description of i.MX8MQ low power modes one can look at
AN12118 i.MX 8M Quad Power Consumption Measurement
sect.2.5.1 Low Level Power Management (PM), sect.2.5.1.3 Source Code Structure
Best regards
igor