imx8dx lpddr4 DDR Stress Test

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

imx8dx lpddr4 DDR Stress Test

2,334 次查看
songhongliang
Contributor II

HI

I use Newest MX8DualX_C0_B0_LPDDR4_RPA_1.2GHz_v15.xlsx to DDR Stress Test。I set the corresponding parameters of LPDDR4 and used the MX8_DDR_Tester.exe tool to test.The test result is not what I want.

I set 1GB(8Gb) in MX8DualX_C0_B0_LPDDR4_RPA_1.2GHz_v15.xlsx,then use the Stress Test Script CBT to test ,I found the MX8_DDR_Tester.exe log Display only 512MB。

How can I get the correct log, can you give me some help?

thanks!

0 项奖励
回复
3 回复数

2,325 次查看
igorpadykov
NXP Employee
NXP Employee

Hi songhongliang

 

for H9HCNNN8KUMLHR part settings may be as below

 

H9HCNNN8KUMLHR.jpg

 

Best regards
igor

0 项奖励
回复

2,321 次查看
songhongliang
Contributor II

HI ,

I mean, the DRAM used is 1GB, and there is only one die ?

thanks!

0 项奖励
回复

2,322 次查看
songhongliang
Contributor II

HI,

if I want use 1GB DRAM,In imx8dx,the LPDDR4 must per die is 1GB?

Thanks

0 项奖励
回复