imx8dx libsdl2 color display problem

キャンセル
次の結果を表示 
次の代わりに検索 
もしかして: 

imx8dx libsdl2 color display problem

219件の閲覧回数
songhongliang
Contributor II

HI

I am trying to use libsdl2, but the windows created with SDL2 on the imx8dx development board are showing wrong colors. Compared with using the same program on ubuntu, the display on Ubuntu is normal, and the color displayed on the imx8dx development board is always wrong. I added in conf/local.conf IMAGE_INSTALL_append += "libsdl2 libsdl2-net libsdl2-mixer libsdl2-ttf libsdl2-image"

 

Thanks!

ラベル(1)
0 件の賞賛
2 返答(返信)

188件の閲覧回数
Sanket_Parekh
NXP Employee
NXP Employee

Hi @songhongliang 

I hope you are doing well.

Please try with libsdl.

Thanks & Regards

Sanket Parekh

0 件の賞賛

217件の閲覧回数
songhongliang
Contributor II

hi

Attached is the comparison shown above on Ubuntu and imx8dx

Thanks

タグ(1)
0 件の賞賛