Hi
now i use command
cat /sys/kernel/debug/dri/1/state
find this: color-encoding=ITU-R BT.601 YCbCr
plane[37]: plane-2
crtc=crtc-2
fb=48
allocated by = weston
refcount=2
format=XR24 little-endian (0x34325258)
modifier=0x0
size=1920x1080
layers:
size[0]=1920x1080
pitch[0]=7680
offset[0]=0
obj[0]:
name=0
refcount=4
start=001017bb
size=8294400
imported=no
paddr=0x00000000d5a00000
vaddr=00000000797290c0
crtc-pos=1920x1080+0+0
src-pos=1920.000000x1080.000000+0.000000+0.000000
rotation=1
normalized-zpos=0
color-encoding=ITU-R BT.601 YCbCr
color-range=YCbCr limited range
connector[41]: HDMI-A-1
crtc=crtc-2
self_refresh_aware=0And i find the problem, my sensor flow(BT.709) save in the USB Disk with format BT.709. is different with the screen i saw on the screen, which is BT.601 format.
Now i want HDMI output BT.709 format instead of BT.601.
Please tell me how to change in the bsp or any other method to modify.
Environment:
CPU: i.MX 8M Plus Quad
Linux version 5.10.9
aarch64-poky-linux-gcc (GCC) 10.2.0,
Thanks a lot.
Hi @Jerry_z
It can not be modified by yourself, It depends on the HDMI spec 2.0, So you can check it on the HDMI spec file.
B.R
hello?
Anyone can answer it ?