Hi
now i use command
cat /sys/kernel/debug/dri/1/state
find this: color-encoding=ITU-R BT.601 YCbCr
plane[37]: plane-2
crtc=crtc-2
fb=48
allocated by = weston
refcount=2
format=XR24 little-endian (0x34325258)
modifier=0x0
size=1920x1080
layers:
size[0]=1920x1080
pitch[0]=7680
offset[0]=0
obj[0]:
name=0
refcount=4
start=001017bb
size=8294400
imported=no
paddr=0x00000000d5a00000
vaddr=00000000797290c0
crtc-pos=1920x1080+0+0
src-pos=1920.000000x1080.000000+0.000000+0.000000
rotation=1
normalized-zpos=0
color-encoding=ITU-R BT.601 YCbCr
color-range=YCbCr limited range
connector[41]: HDMI-A-1
crtc=crtc-2
self_refresh_aware=0
And i find the problem, my sensor flow(BT.709) save in the USB Disk with format BT.709. is different with the screen i saw on the screen, which is BT.601 format.
Now i want HDMI output BT.709 format instead of BT.601.
Please tell me how to change in the bsp or any other method to modify.
Environment:
CPU: i.MX 8M Plus Quad
Linux version 5.10.9
aarch64-poky-linux-gcc (GCC) 10.2.0,
Thanks a lot.