imx8MP ERROR: imx-image-full-1.0-r0 do_rootfs

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx8MP ERROR: imx-image-full-1.0-r0 do_rootfs

1,071 Views
gopalambike1
Contributor I

Build Configuration:
BB_VERSION = "2.8.0"
BUILD_SYS = "x86_64-linux"
NATIVELSBSTRING = "universal"
TARGET_SYS = "aarch64-poky-linux"
MACHINE = "imx8mp-lpddr4-evk"
DISTRO = "fsl-imx-xwayland"
DISTRO_VERSION = "6.6-scarthgap"
TUNE_FEATURES = "aarch64 armv8a crc crypto"
TARGET_FPU = ""
meta
meta-poky = "HEAD:02eacd385eca7aa9cf25aaaa61427aa9c126e0bc"
meta-oe
meta-multimedia
meta-python = "HEAD:a72010b414ee3d73888ac9cb4e310e8f05e13aea"
meta-freescale = "HEAD:41b923e59e048b9b2942ff737a4ddac386954c62"
meta-freescale-3rdparty = "HEAD:8b61684f0b1ba8bacdf3a69d993445e9791d4932"
meta-freescale-distro = "HEAD:158cc55b6ee30d09957b380859dba52c0f6af68d"
meta-imx-bsp
meta-imx-sdk
meta-imx-ml
meta-imx-v2x = "HEAD:ae04eecd48e557437ec90366795b8cf202d0ce14"
meta-nxp-demo-experience = "HEAD:5c0d6796620b911f7445da5537a6d71cb9764ab4"
meta-nxp-matter-baseline
meta-nxp-openthread = "HEAD:96311d23e51ddd76cfa73a8bbd65b13c82ab5f7d"
meta-arm
meta-arm-toolchain = "HEAD:8aa8a1f17f5b64bc691544f989f04fc83df98adb"
meta-chromium = "HEAD:dc31889c0899971def535dc1c040edf18bc16691"
meta-clang = "HEAD:66414c17ae60e489bef9a97031323e92c247fbe1"
meta-gnome
meta-networking
meta-filesystems = "HEAD:a72010b414ee3d73888ac9cb4e310e8f05e13aea"
meta-qt6 = "HEAD:dc13e1bfda4a4757a08c2d6673bc4bac012c4a80"
meta-parsec
meta-tpm = "HEAD:11ea91192d43d7c2b0b95a93aa63ca7e73e38034"
meta-virtualization = "HEAD:1a547c0aa0d75c4143cbb66de6e653d51cdc8bda"

Sstate summary: Wanted 3 Local 0 Mirrors 0 Missed 3 Current 7701 (0% match, 99% complete)
Initialising tasks: 100% |#######################################| Time: 0:00:09
NOTE: Executing Tasks
ERROR: imx-image-full-1.0-r0 do_rootfs: Unable to install packages. Command '/home/intellipredikt/imx-yocto/intellipredikt/tmp/work/imx8mp_lpddr4_evk-poky-linux/imx-image-full/1.0/recipe-sysroot-native/usr/bin/apt-get install --allow-downgrades --allow-remove-essential --allow-change-held-packages --allow-unauthenticated --no-remove apt curl docker dpkg firmwared imx-g2d-samples jailhouse opencv-apps opencv-samples optee-client optee-os os-release packagegroup-base-extended packagegroup-core-boot packagegroup-core-full-cmdline packagegroup-core-nfs-client packagegroup-core-sdk packagegroup-core-ssh-openssh packagegroup-core-standalone-sdk-target packagegroup-core-tools-debug packagegroup-core-tools-profile packagegroup-core-tools-testapps packagegroup-core-weston packagegroup-fsl-gstreamer1.0 packagegroup-fsl-gstreamer1.0-full packagegroup-fsl-optee-imx packagegroup-fsl-tools-audio packagegroup-fsl-tools-benchmark packagegroup-fsl-tools-gpu packagegroup-fsl-tools-gpu-external packagegroup-fsl-tools-testapps packagegroup-imx-isp packagegroup-imx-ml packagegroup-imx-security packagegroup-qt6-imx packagegroup-security-parsec packagegroup-security-tpm2 packagegroup-tools-bluetooth psplash python3-opencv run-postinsts softhsm swtpm tzdata weston-xwayland xterm' returned 100:
Reading package lists...
Building dependency tree...
Reading state information...
Some packages could not be installed. This may mean that you have
requested an impossible situation or if you are using the unstable
distribution that some required packages have not yet been created
or been moved out of Incoming.
The following information may help to resolve the situation:

The following packages have unmet dependencies:
imx-gpu-sdk : Depends: gli but it is not installable
Depends: glm but it is not installable
Depends: googletest but it is not installable
Depends: libfmt10 (>= 10.2.1) but it is not installable
Depends: libvulkan1 (>= 1.3.275.0) but it is not installable
Depends: pugixml but it is not installable
Depends: rapidjson but it is not installable
Depends: rapidopenvx but it is not installable
libgtk-2.0 : Depends: libxrandr2 (>= 1.5.4) but it is not installable
Recommends: gdk-pixbuf-loader-jpeg but it is not installable
Recommends: gdk-pixbuf-loader-png but it is not installable
Recommends: gnome-theme-adwaita but it is not going to be installed
qtbase : Depends: vulkan-loader but it is not installable
Recommends: qtbase-plugins but it is not going to be installed
Recommends: qtbase-qmlplugins but it is not going to be installed
vkmark : Depends: libvulkan1 (>= 1.3.275.0) but it is not installable
vulkan-validation-layers : Depends: spirv-tools (>= 1.3.275.0) but it is not installable
E: Unable to correct problems, you have held broken packages.

ERROR: Logfile of failure stored in: /home/intellipredikt/imx-yocto/intellipredikt/tmp/work/imx8mp_lpddr4_evk-poky-linux/imx-image-full/1.0/temp/log.do_rootfs.123129
ERROR: Task (/home/intellipredikt/imx-yocto/sources/meta-imx/meta-imx-sdk/dynamic-layers/qt6-layer/recipes-fsl/images/imx-image-full.bb:do_rootfs) failed with exit code '1'

Labels (1)
0 Kudos
Reply
0 Replies