imx8MM mini EVK kit U-boot splash screen does not appear consistently on power up

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx8MM mini EVK kit U-boot splash screen does not appear consistently on power up

1,381 Views
KJ_Mehta
Contributor I
In U-boot code, splash screen (default NXP Logo) we were able to see on the HDMI screen thro' Adapter provided by NXP.
    but, we observed one issue.
  • During Power on/off through (on/off switch on the imx8MM mini board), the NXP splash screen logo does not come up consistently. Almost every time it misses appearance on the screen but we observe Linux Penguin logo every time consistently.
  • Once the system is powered up, and if we do manual 'reset' button on board, or from linux-$ reboot cmd  then the splash screen is always visisble after reboot.So this behaviour is not understood clearly so far. 
  • if we stop the boot up process (say press ctrl-C) and get to u-boot prompt then also NXP splash screen is visible always.   
Power on/off (power recycle) is the usual way of starting the system, so this inconsistent behavior will be an issue for us going forward. please let us know any solutions or reasons of this behavior.
 
At present, we are using the following items:
Imx8mm Mini EVK board,  NXP provided HDMI Adapter and its SAS cable and we have a 21" LCD display screen (Benq make). We do not have MIPI display with us.
 
Regards,
Krishnakant Mehta
 
0 Kudos
Reply
3 Replies

521 Views
sachindsilva16
Contributor I

Could you please provide me the procedure that you followed to display and render the penguin logo during linux boot for imx8MM mini board? I appreciate your kind support.
Thank you in advance.

Regards,
Sachin

0 Kudos
Reply

1,370 Views
KJ_Mehta
Contributor I

Yes, we are using Imx8MM mini EVK and MIPI to HDMI adapter board and output is connected to HDMI LCD screen (21").

 

 

0 Kudos
Reply

1,374 Views
Zhiming_Liu
NXP TechSupport
NXP TechSupport

You are using EVK+ MIPI to HDMI board ,right?

0 Kudos
Reply