imx8 yocto pulseaudio doesn't work for gstreamer

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

imx8 yocto pulseaudio doesn't work for gstreamer

3,650 次查看
Anton_K
Contributor III

Hello!
I have some problems with pulseaudio for gst-launch-1.0.

Actually I can use simple command line test with following logs:

 

$> GST_DEBUG=3,pulse*:9 gst-launch-1.0 pulsesrc ! autoaudiosink
Setting pipeline to PAUSED ...
0:00:00.146182796   732 0xaaaab6d3fb30 DEBUG                  pulse pulsesink.c:2226:gst_pulsesink_query_getcaps:<autoaudiosink0-actual-sink-pulse> caps audio/x-raw, format=(string){ S16LE, S16BE, F32LE, F32BE, S32LE, S32BE, S24LE, S24BE, S24_32LE, S24_32BE, U8 }, layout=(string)interleaved, rate=(int)[ 1, 384000 ], channels=(int)[ 1, 32 ]; audio/x-alaw, rate=(int)[ 1, 384000 ], channels=(int)[ 1, 32 ]; audio/x-mulaw, rate=(int)[ 1, 384000 ], channels=(int)[ 1, 32 ]; audio/x-ac3, framed=(boolean)true; audio/x-eac3, framed=(boolean)true; audio/x-dts, framed=(boolean)true, block-size=(int){ 512, 1024, 2048 }; audio/mpeg, mpegversion=(int)1, mpegaudioversion=(int)[ 1, 3 ], parsed=(boolean)true; audio/mpeg, mpegversion=(int){ 2, 4 }, framed=(boolean)true, stream-format=(string)adts
0:00:00.146336422   732 0xaaaab6d3fb30 INFO                   pulse pulsesink.c:3254:gst_pulsesink_change_state:<autoaudiosink0-actual-sink-pulse> new pa main loop thread
0:00:00.146838551   732 0xaaaab6d3fb30 DEBUG                  pulse pulsesink.c:1836:gst_pulsesink_create_ringbuffer:<autoaudiosink0-actual-sink-pulse> creating ringbuffer
0:00:00.147029803   732 0xaaaab6d3fb30 DEBUG                  pulse pulsesink.c:1838:gst_pulsesink_create_ringbuffer:<autoaudiosink0-actual-sink-pulse> created ringbuffer @0xaaaab6e40030
0:00:00.147105553   732 0xaaaab6d3fb30 INFO                   pulse pulsesink.c:533:gst_pulseringbuffer_open_device:<autoaudiosink0-actual-sink-pulse> new context with name gst-launch-1.0, pbuf=0xaaaab6e40030, pctx=0xaaaab6e26980
0:00:00.148039936   732 0xaaaab6d3fb30 LOG                    pulse pulsesink.c:550:gst_pulseringbuffer_open_device:<autoaudiosink0-actual-sink-pulse> connect to server (NULL)
0:00:00.148443189   732 0xaaaab6d3fb30 LOG                    pulse pulsesink.c:427:gst_pulsering_context_state_cb: got new context state 1
0:00:00.152361345   732 0xaaaab6d3fb30 LOG                    pulse pulsesink.c:427:gst_pulsering_context_state_cb: got new context state 5
0:00:00.152458346   732 0xaaaab6d3fb30 LOG                    pulse pulsesink.c:433:gst_pulsering_context_state_cb: signaling
0:00:00.152554472   732 0xaaaab6d3fb30 WARN                   pulse pulsesink.c:617:gst_pulseringbuffer_open_device:<autoaudiosink0-actual-sink-pulse> error: Failed to connect: Connection refused
0:00:00.152844599   732 0xaaaab6d3fb30 DEBUG                  pulse pulsesink.c:340:gst_pulsering_destroy_context:<pulseringbuffer0> destroying ringbuffer 0xaaaab6e40030
0:00:00.152908100   732 0xaaaab6d3fb30 DEBUG                  pulse pulsesink.c:354:gst_pulsering_destroy_context:<pulseringbuffer0> releasing context with name gst-launch-1.0, pbuf=0xaaaab6e40030, pctx=0xaaaab6e26980
0:00:00.152959725   732 0xaaaab6d3fb30 DEBUG                  pulse pulsesink.c:360:gst_pulsering_destroy_context:<pulseringbuffer0> destroying final context with name gst-launch-1.0, pbuf=0xaaaab6e40030, pctx=0xaaaab6e26980
0:00:00.153154977   732 0xaaaab6d3fb30 DEBUG                  pulse pulsesink.c:340:gst_pulsering_destroy_context:<pulseringbuffer0> destroying ringbuffer 0xaaaab6e40030
0:00:00.153214352   732 0xaaaab6d3fb30 INFO                   pulse pulsesink.c:3236:gst_pulsesink_release_mainloop:<autoaudiosink0-actual-sink-pulse> terminating pa main loop thread
0:00:00.231180477   732 0xaaaab6d3fb30 DEBUG                  pulse pulsesrc.c:997:gst_pulsesrc_open:<pulsesrc0> opening device
0:00:00.231943233   732 0xaaaab6d3fb30 DEBUG                  pulse pulsesrc.c:1012:gst_pulsesrc_open:<pulsesrc0> connect to server (NULL)
0:00:00.236367893   732 0xaaaab6d3fb30 WARN                   pulse pulsesrc.c:1016:gst_pulsesrc_open:<pulsesrc0> error: Failed to connect: Connection refused
ERROR: from element /GstPipeline:pipeline0/GstPulseSrc:pulsesrc0: Failed to connect: Connection refused
Additional debug info:
../git/ext/pulse/pulsesrc.c(1016): gst_pulsesrc_open (): /GstPipeline:pipeline0/GstPulseSrc:pulsesrc0
ERROR: pipeline doesn't want to preroll.
Failed to set pipeline to PAUSED.
Setting pipeline to NULL ...
Freeing pipeline ...

 

 I have no idea what audio server needs for pulsesrc, probably it needs some /dev/audioX, but on this machine there is no /dev/audioX available, may be there is some issue here.

Also I have this audio devices on gst-device-monitor-1.0:

root@imx8qxp-var-som:~# gst-device-monitor-1.0 
Probing devices...


(gst-device-monitor-1.0:520): GStreamer-CRITICAL **: 08:36:22.486: gst_element_message_full_with_details: assertion 'GST_IS_ELEMENT (element)' failed

(gst-device-monitor-1.0:520): GStreamer-CRITICAL **: 08:36:22.499: gst_element_message_full_with_details: assertion 'GST_IS_ELEMENT (element)' failed

...

Device found:

	name  : wm8904-audio
	class : Audio/Sink
	caps  : audio/x-raw, format={ (string)S32LE, (string)S24_32LE, (string)S16LE }, layout=interleaved, rate=[ 8000, 96000 ], channels=2, channel-mask=0x0000000000000003
	properties:
		device.api = alsa
		device.class = sound
		alsa.card = 0
		alsa.card_name = wm8904-audio
		alsa.driver_name = simple-card
		alsa.name = wm8904-audio
		alsa.id = wm8904audio
		alsa.mixername = ""
		alsa.components = ""
	gst-launch-1.0 ... ! alsasink device="hw:0\,0"


Device found:

	name  : wm8904-audio
	class : Audio/Source
	caps  : audio/x-raw, format={ (string)S32LE, (string)S24_32LE, (string)S16LE }, layout=interleaved, rate=[ 8000, 96000 ], channels=2, channel-mask=0x0000000000000003
	properties:
		device.api = alsa
		device.class = sound
		alsa.card = 0
		alsa.card_name = wm8904-audio
		alsa.driver_name = simple-card
		alsa.name = wm8904-audio
		alsa.id = wm8904audio
		alsa.mixername = ""
		alsa.components = ""
	gst-launch-1.0 alsasrc device="hw:0\,0" ! ...


I have tried also with alsasrc record and play:

root@imx8qxp-var-som:~# GST_DEBUG=3,alsa*:9 gst-launch-1.0 -v alsasrc device="hw:0,0" ! audioconvert ! vorbisenc ! oggmux ! filesink location=alsasrc.ogg
0:00:00.123746529   864 0xaaaafccd5c70 DEBUG                   alsa gstalsaelement.c:70:alsa_element_init: binding text domain gst-plugins-base-1.0 to locale dir /usr/share/locale
0:00:00.125168673   864 0xaaaafccd5c70 DEBUG                   alsa gstalsasrc.c:300:gst_alsasrc_init:<GstAlsaSrc@0xaaaafcdb8270> initializing
0:00:00.140407715   864 0xaaaafccd5c70 DEBUG                   alsa gstalsasrc.c:328:gst_alsasrc_getcaps:<alsasrc0> device not open, using template caps
0:00:00.140810881   864 0xaaaafccd5c70 DEBUG                   alsa gstalsasrc.c:328:gst_alsasrc_getcaps:<alsasrc0> device not open, using template caps
0:00:00.141142165   864 0xaaaafccd5c70 DEBUG                   alsa gstalsasrc.c:328:gst_alsasrc_getcaps:<alsasrc0> device not open, using template caps
0:00:00.141795106   864 0xaaaafccd5c70 DEBUG                   alsa gstalsasrc.c:328:gst_alsasrc_getcaps:<alsasrc0> device not open, using template caps
Setting pipeline to PAUSED ...
Pipeline is live and does not need PREROLL ...
0:00:00.155190712   864 0xaaaafcb23b60 FIXME                default gstutils.c:4025:gst_pad_create_stream_id_internal:<alsasrc0:src> Creating random stream-id, consider implementing a deterministic way of creating a stream-id
0:00:00.155554499   864 0xaaaafcb23b60 INFO                    alsa gstalsasrc.c:346:gst_alsasrc_getcaps:<alsasrc0> template caps audio/x-raw, format=(string){ F64LE, F64BE, F32LE, F32BE, S32LE, S32BE, U32LE, U32BE, S24_32LE, S24_32BE, U24_32LE, U24_32BE, S24LE, S24BE, U24LE, U24BE, S20LE, S20BE, U20LE, U20BE, S18LE, S18BE, U18LE, U18BE, S16LE, S16BE, U16LE, U16BE, S8, U8 }, layout=(string)interleaved, rate=(int)[ 1, 2147483647 ], channels=(int)[ 1, 2147483647 ]; audio/x-iec958, format=(string)U32LE, layout=(string)interleaved, rate=(int)[ 1, 2147483647 ], channels=(int)2
0:00:00.155851654   864 0xaaaafcb23b60 DEBUG                   alsa gstalsa.c:196:gst_alsa_detect_formats:<alsasrc0> audio/x-iec958
Pipeline is PREROLLED ...
Setting pipeline to PLAYING ...
0:00:00.155952789   864 0xaaaafcb23b60 LOG                     alsa gstalsa.c:30:gst_alsa_detect_rates:<alsasrc0> probing sample rates ...
0:00:00.156008295   864 0xaaaafcb23b60 DEBUG                   alsa gstalsa.c:49:gst_alsa_detect_rates:<alsasrc0> Min. rate = 8000 (8000)
0:00:00.156054924   864 0xaaaafcb23b60 DEBUG                   alsa gstalsa.c:50:gst_alsa_detect_rates:<alsasrc0> Max. rate = 96000 (96000)
0:00:00.156100804   864 0xaaaafcb23b60 LOG                     alsa gstalsa.c:372:gst_alsa_detect_channels:<alsasrc0> probing channels ...
0:00:00.156161685   864 0xaaaafcb23b60 DEBUG                   alsa gstalsa.c:416:gst_alsa_detect_channels:<alsasrc0> Min. channels = 2 (2)
0:00:00.156208315   864 0xaaaafcb23b60 DEBUG                   alsa gstalsa.c:417:gst_alsa_detect_channels:<alsasrc0> Max. channels = 2 (2)
0:00:00.156328827   864 0xaaaafcb23b60 INFO                    alsa gstalsasrc.c:356:gst_alsasrc_getcaps:<alsasrc0> returning caps audio/x-raw, format=(string){ S32LE, S24_32LE, S16LE }, layout=(string)interleaved, rate=(int)[ 8000, 96000 ], channels=(int)2, channel-mask=(bitmask)0x0000000000000003
New clock: GstAudioSrcClock
0:00:00.158278400   864 0xaaaafcb23b60 DEBUG                   alsa gstalsasrc.c:406:set_hwparams:<alsasrc0> buffer time 200000, min 2993, max 2972155
0:00:00.158365408   864 0xaaaafcb23b60 DEBUG                   alsa gstalsasrc.c:412:set_hwparams:<alsasrc0> period time 10000, min 1496, max 185715
0:00:00.158448292   864 0xaaaafcb23b60 DEBUG                   alsa gstalsasrc.c:418:set_hwparams:<alsasrc0> periods min 2, max 1985
0:00:00.158584931   864 0xaaaafcb23b60 DEBUG                   alsa gstalsasrc.c:433:set_hwparams:<alsasrc0> period time 10068 buffer time 201360 set correctly
0:00:00.182139690   864 0xaaaafcb23b60 DEBUG                   alsa gstalsasrc.c:478:set_hwparams:<alsasrc0> buffer size : 8880
0:00:00.182233075   864 0xaaaafcb23b60 DEBUG                   alsa gstalsasrc.c:481:set_hwparams:<alsasrc0> period size : 444
0:00:00.182459348   864 0xaaaafcb23b60 DEBUG                   alsa gstalsasrc.c:834:gst_alsasrc_prepare:<alsasrc0> Hardware setup: 
  stream       : CAPTURE
  access       : RW_INTERLEAVED
  format       : S16_LE
  subformat    : STD
  channels     : 2
  rate         : 44100
  exact rate   : 44100 (44100/1)
  msbits       : 16
  buffer_size  : 8880
  period_size  : 444
  period_time  : 10068

0:00:00.182580360   864 0xaaaafcb23b60 DEBUG                   alsa gstalsasrc.c:839:gst_alsasrc_prepare:<alsasrc0> Software setup: 
  tstamp_mode  : ENABLE
  tstamp_type  : MONOTONIC
  period_step  : 1
  avail_min    : 444
  period_event : 0
  start_threshold  : 0
  stop_threshold   : 8880
  silence_threshold: 0
  silence_size : 0
  boundary     : 4998995586381250560

0:00:00.182830135   864 0xaaaafcb23b60 WARN                    alsa pcm_hw.c:1360:snd_pcm_hw_get_chmap: alsalib error: Cannot read Channel Map ctl
: No such file or directory
0:00:00.182935146   864 0xaaaafcb23b60 LOG                     alsa gstalsa.c:860:alsa_detect_channels_mapping:<alsasrc0> ALSA driver does not implement channels mapping API
/GstPipeline:pipeline0/GstAlsaSrc:alsasrc0: actual-buffer-time = 201360
/GstPipeline:pipeline0/GstAlsaSrc:alsasrc0: actual-latency-time = 10068
Redistribute latency...
/GstPipeline:pipeline0/GstAlsaSrc:alsasrc0.GstPad:src: caps = audio/x-raw, format=(string)S16LE, layout=(string)interleaved, rate=(int)44100, channels=(int)2, channel-mask=(bitmask)0x0000000000000003
/GstPipeline:pipeline0/GstAudioConvert:audioconvert0.GstPad:src: caps = audio/x-raw, rate=(int)44100, channels=(int)2, format=(string)F32LE, layout=(string)interleaved, channel-mask=(bitmask)0x0000000000000003
/GstPipeline:pipeline0/GstVorbisEnc:vorbisenc0.GstPad:sink: caps = audio/x-raw, rate=(int)44100, channels=(int)2, format=(string)F32LE, layout=(string)interleaved, channel-mask=(bitmask)0x0000000000000003
/GstPipeline:pipeline0/GstAudioConvert:audioconvert0.GstPad:sink: caps = audio/x-raw, format=(string)S16LE, layout=(string)interleaved, rate=(int)44100, channels=(int)2, channel-mask=(bitmask)0x0000000000000003
/GstPipeline:pipeline0/GstVorbisEnc:vorbisenc0: last-message = encoding at quality level 0.30
Redistribute latency...
0:00:00.246260682   864 0xaaaafcb23b60 FIXME               basesink gstbasesink.c:3395:gst_base_sink_default_event:<filesink0> stream-start event without group-id. Consider implementing group-id handling in the upstream elements
0:00:00.246644846   864 0xaaaafcb23b60 WARN            audioencoder gstaudioencoder.c:980:gst_audio_encoder_finish_frame:<vorbisenc0> Can't copy metadata because input buffer disappeared

Some scope of issues But it tries to record with time counting, then I'm trying to play and no sound on output:

root@imx8qxp-var-som:~# GST_DEBUG=3,alsa*:9 gst-launch-1.0 filesrc location=alsasrc.ogg ! oggdemux ! vorbisdec ! audioconvert ! audioresample ! autoaudiosink
Setting pipeline to PAUSED ...
0:00:00.164507605   885 0xaaab1e302810 WARN                   pulse pulsesink.c:617:gst_pulseringbuffer_open_device:<autoaudiosink0-actual-sink-pulse> error: Failed to connect: Connection refused
0:00:00.169726634   885 0xaaab1e302810 DEBUG                   alsa gstalsaelement.c:70:alsa_element_init: binding text domain gst-plugins-base-1.0 to locale dir /usr/share/locale
0:00:00.170570574   885 0xaaab1e302810 DEBUG                   alsa gstalsasink.c:266:gst_alsasink_init:<GstAlsaSink@0xaaab1e325a30> initializing alsasink
0:00:00.170680208   885 0xaaab1e302810 DEBUG                   alsa gstalsasink.c:308:gst_alsasink_getcaps:<autoaudiosink0-actual-sink-alsa> device not open, using template caps
0:00:00.234804418   885 0xaaab1e302810 LOG                     alsa gstalsasink.c:911:gst_alsasink_open:<autoaudiosink0-actual-sink-alsa> Opened device default
0:00:00.241689951   885 0xaaab1e302810 LOG                     alsa gstalsasink.c:911:gst_alsasink_open:<autoaudiosink0-actual-sink-alsa> Opened device default
0:00:00.243218194   885 0xaaab1e302810 WARN                 basesrc gstbasesrc.c:3688:gst_base_src_start_complete:<filesrc0> pad not activated yet
Pipeline is PREROLLING ...
0:00:00.245038710   885 0xaaab1e3144c0 WARN                oggdemux gstoggdemux.c:3417:gst_ogg_demux_do_seek:<'':src_47b83c1f> Locking on pts 0:00:00.480362811
0:00:00.246162796   885 0xaaab1e3144c0 DEBUG                   alsa gstalsa.c:198:gst_alsa_detect_formats:<autoaudiosink0-actual-sink-alsa> skipping non-raw format or iec958 format
0:00:00.246275055   885 0xaaab1e3144c0 DEBUG                   alsa gstalsa.c:198:gst_alsa_detect_formats:<autoaudiosink0-actual-sink-alsa> skipping non-raw format or iec958 format
0:00:00.246317183   885 0xaaab1e3144c0 DEBUG                   alsa gstalsa.c:198:gst_alsa_detect_formats:<autoaudiosink0-actual-sink-alsa> skipping non-raw format or iec958 format
0:00:00.246358937   885 0xaaab1e3144c0 DEBUG                   alsa gstalsa.c:198:gst_alsa_detect_formats:<autoaudiosink0-actual-sink-alsa> skipping non-raw format or iec958 format
0:00:00.246417816   885 0xaaab1e3144c0 LOG                     alsa gstalsa.c:30:gst_alsa_detect_rates:<autoaudiosink0-actual-sink-alsa> probing sample rates ...
0:00:00.246481696   885 0xaaab1e3144c0 DEBUG                   alsa gstalsa.c:49:gst_alsa_detect_rates:<autoaudiosink0-actual-sink-alsa> Min. rate = 4000 (4000)
0:00:00.246528575   885 0xaaab1e3144c0 DEBUG                   alsa gstalsa.c:50:gst_alsa_detect_rates:<autoaudiosink0-actual-sink-alsa> Max. rate = 2147483647 (-1)
0:00:00.246574578   885 0xaaab1e3144c0 LOG                     alsa gstalsa.c:372:gst_alsa_detect_channels:<autoaudiosink0-actual-sink-alsa> probing channels ...
0:00:00.246624707   885 0xaaab1e3144c0 DEBUG                   alsa gstalsa.c:416:gst_alsa_detect_channels:<autoaudiosink0-actual-sink-alsa> Min. channels = 1 (1)
0:00:00.246670836   885 0xaaab1e3144c0 DEBUG                   alsa gstalsa.c:417:gst_alsa_detect_channels:<autoaudiosink0-actual-sink-alsa> Max. channels = 8 (10000)
0:00:00.247879554   885 0xaaab1e3144c0 DEBUG                   alsa gstalsa.c:498:gst_alsa_open_iec958_pcm:<autoaudiosink0-actual-sink-alsa> Generated device string "default"
0:00:00.257634559   885 0xaaab1e3144c0 LOG                     alsa gstalsasink.c:348:gst_alsasink_getcaps:<autoaudiosink0-actual-sink-alsa> Add pass-through capabilities
...


Also I can test output sound and it works, like:

root@imx8qxp-var-som:~# gst-launch-1.0 audiotestsrc ! autoaudiosink

So the issue on the source audio device

Also I can run another Linux image and micro also works

My system configuration:
Custom yocto distro Linux imx8qxp-var-som 5.15.60 Kirkstone 

Let me summarize the yocto configuration:

DISTRO_FEATURES_BACKFILL_CONSIDERED:remove = " pulseaudio"
DISTRO_FEATURES_BACKFILL:append = " pulseaudio"
DISTRO_FEATURES:append = " alsa"


Can someone help me to resolve the problem on audio source solution. It doesn't matter use pulsesrc or alsasrc.
Thanks in advance, Anton

0 项奖励
回复
5 回复数

3,619 次查看
joanxie
NXP TechSupport
NXP TechSupport

pls try this:

The pipeline described below shows the process to obtain this type of audio file and save it as an Ogg Vorbis file:
$ gst-launch-1.0 -v pulsesrc ! audioconvert ! vorbisenc ! oggmux ! filesink location=alsasrc.ogg

0 项奖励
回复

3,610 次查看
Anton_K
Contributor III

Hello, the result of command will be the same as on the first code block on my question before. The issue:

<autoaudiosink0-actual-sink-pulse> error: Failed to connect: Connection refused

 

I've made some progress and suppose that I have no configuration for micro.
Can you help me to configure micro input for the yocto build? Totally I have connected micro to the right channel on the LINEIN1_RP pin on the var-som-mx8x

0 项奖励
回复

3,546 次查看
joanxie
NXP TechSupport
NXP TechSupport

since you use the third party company bsp, suggest that you can compare your bsp with nxp bsp, which can support this already

0 项奖励
回复

3,538 次查看
Anton_K
Contributor III
Thank you for your time, will do. I just mean, have I done enough in distro recipes to include "pulseaudio" correctly related to this issue?
0 项奖励
回复

3,488 次查看
joanxie
NXP TechSupport
NXP TechSupport
0 项奖励
回复