imx8 with ubuntu ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx8 with ubuntu ?

5,660 Views
rans
Senior Contributor I

Hello,

Is it possible to use ubuntu with imx8 ?

What's the best method to do it ? Is it that the imx6 ubuntu tutorial (https://community.nxp.com/docs/DOC-330147 ) Can be used for imx8 too ?

Thanks

3 Replies

3,538 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hi ranshalit,

Unfortunately, we do not have support for Ubuntu for i.MX8 devices. I apologize for the inconveniences this could give you.

In mean time you can check the Ubuntu for MX8M from Boundary Devices:

Ubuntu Bionic 18.04 LTS for Nitrogen8M board – September 2018 (kernel 4.9.x) - Boundary Devices 

 

Regards

3,538 Views
rans
Senior Contributor I

Hi

Thanks for the reply.

Is there any plan to add it in the future?

Thanks

0 Kudos
Reply

3,538 Views
jerry2
Contributor II
0 Kudos
Reply