imx8 wayland qt qml can not use yuv camera

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

imx8 wayland qt qml can not use yuv camera

2,287 次查看
songhongliang
Contributor II

HI,

I want to use QT's QCamera or QML to get the video display, but it is currently not successful.

I use           gst-launch-1.0 imxcompositor_g2d v4l2src device=/dev/video8!'Video/x-raw,format=RGB16,framerate=25/1,width=1280,height=720'! Autovideosink     is ok,

but I am more I want to use QCmaera or QML directly.

In the test, the usb camera can be directly called with QCmera or QML。

thanks

标签 (2)
0 项奖励
回复
5 回复数

2,280 次查看
joanxie
NXP TechSupport
NXP TechSupport

what imx8 board do you mean?

0 项奖励
回复

2,277 次查看
songhongliang
Contributor II

HI joanxie

it is imx8qm board,

I usb QT QCamera or qml  can not use ISI registered  /dev/videox,

but the uvc video is ok。

you can look this,I think they should be the same problem

ommunity.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX-8-8X-Family-DDR-Tools-Release/ta-p/1121519

0 项奖励
回复

2,257 次查看
joanxie
NXP TechSupport
NXP TechSupport

yes it seems ths exit issue of qt camera on imx8qm or imx8qxp, because the DPU DC overlay plane can support tile format. if you use gstreamer, you need to use g2d convert tile to linear, so the expert team suggst customer to use gstreamer which is supported by them, qt multimedia isn't

0 项奖励
回复

2,229 次查看
songhongliang
Contributor II

HI 

I need to display 3 camera images in qt, but it is not very smooth at the moment, is there a routine for using gst to call multiple cameras in qt

Thanks

0 项奖励
回复

2,251 次查看
songhongliang
Contributor II

HI,

I look forward to supporting qtmultimedia in the future, so development and use will be very convenient.

thanks

0 项奖励
回复