imx8 wakeup on canbus activity

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

imx8 wakeup on canbus activity

2,028 次查看
agmc1971
Contributor I

Hello,

I would like to resume from suspend using canbus activity , do someone have already managed this?

In the case, is it also possible to read the packets that arrived from canbus or are they lost?

Thanks in advance

BR

 

0 项奖励
回复
4 回复数

2,015 次查看
igorpadykov
NXP Employee
NXP Employee

Hi agmc1971

 

for canbus wake example one can look at "power_mode_switch" demo included in

MCUXpresso M4 SDK_MEK-MIMX8QX

https://mcuxpresso.nxp.com/en/welcome

 

Best regards
igor

0 项奖励
回复

2,005 次查看
agmc1971
Contributor I

Hi Igor,

thanks for your answer.

Do you think that also IMX6 processors can manage such scenario ( wakeup from can activity), too?

I am evaluating the right platform for my application.

Thanks a lot

 

0 项奖励
回复

1,997 次查看
igorpadykov
NXP Employee
NXP Employee

Hi agmc1971

 

yes i.MX6 processors support it too.

 

Best regards
igor

0 项奖励
回复

1,992 次查看
agmc1971
Contributor I

thankyou very much Igor!

Have a nice day.

0 项奖励
回复