imx8 wakeup on canbus activity

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx8 wakeup on canbus activity

1,883件の閲覧回数
agmc1971
Contributor I

Hello,

I would like to resume from suspend using canbus activity , do someone have already managed this?

In the case, is it also possible to read the packets that arrived from canbus or are they lost?

Thanks in advance

BR

 

0 件の賞賛
返信
4 返答(返信)

1,870件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi agmc1971

 

for canbus wake example one can look at "power_mode_switch" demo included in

MCUXpresso M4 SDK_MEK-MIMX8QX

https://mcuxpresso.nxp.com/en/welcome

 

Best regards
igor

0 件の賞賛
返信

1,860件の閲覧回数
agmc1971
Contributor I

Hi Igor,

thanks for your answer.

Do you think that also IMX6 processors can manage such scenario ( wakeup from can activity), too?

I am evaluating the right platform for my application.

Thanks a lot

 

0 件の賞賛
返信

1,852件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi agmc1971

 

yes i.MX6 processors support it too.

 

Best regards
igor

0 件の賞賛
返信

1,847件の閲覧回数
agmc1971
Contributor I

thankyou very much Igor!

Have a nice day.

0 件の賞賛
返信