imx8 surround-view-3D_1.1_beta calibration application issue (AXI BUS ERROR)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

imx8 surround-view-3D_1.1_beta calibration application issue (AXI BUS ERROR)

560 次查看
songhongliang
Contributor II

HI

I'm trying to use surround-view-3D_1.1_beta and when I run the compiled calibration app auto_calib_1.1 I get an error.I don't know where this is the problem, let's see where the problem is. 

[21599.603926] input fmt YUV4
[21599.607768] output fmt YUYV
[21599.949194] AXI BUS ERROR
[21599.951845] GPU[0](ChipModel=0x7000 ChipRevision=0x6214):
[21599.957308] **************************
[21599.961120] *** GPU STATE DUMP ***
[21599.964902] **************************
[21599.968677] axi = 0x000000A7
[21599.972182] idle = 0x7FFFFFFE
[21599.975673] FE not idle
[21599.978493] DMA address is constant, but state is changing:
[21599.984273] 0x00000000
[21599.986984] 0x00000200
[21599.989718] dmaLow = 0x40000002
[21599.993229] dmaHigh = 0x98901BF8
[21599.996746] dmaState = 0x00000200
[21600.000260] command state = 0 (PAR_IDLE_ST)
[21600.005337] command DMA state = 2 (CMD_REQ_ST)
[21600.010338] command fetch state = 0 (FET_IDLE_ST)
[21600.015425] DMA request state = 0 (REQ_IDLE_ST)
[21600.020511] cal state = 0 (CAL_IDLE_ST)
[21600.025592] VE request state = 0 (VER_IDLE_ST)
[21600.030691] Debug registers:
[21600.033786] RA[0] debug registers:

 

Thanks.

0 项奖励
回复
0 回复数