imx8 quad eth0 and eth1

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx8 quad eth0 and eth1

Jump to solution
4,832 Views
SoftMicro
Contributor II

We have a custom board using an Apalis i.mx8 Quad Max running Android 10

We are trying to use both eth0 and eth1 ports on the custom boards using 2 x KSZ9131 phy's. We can bring up individual phy's OK (ping etc) but cannot bring up and use both phy's.

apalis_8qm:/ # ifconfig eth1 up
[ 281.500581] Microchip KSZ9131 Gigabit PHY 5b050000.ethernet-2:07: attached PHY driver [Microchip KSZ9131 Gigabit PHY] (mii_bus:phy_addr=5b050000.ethernet-2:07, irq=POLL)
apalis_8qm:/ # [ 284.592335] fec 5b050000.ethernet eth1: Link is Up - 100Mbps/Full - flow control rx/tx
[ 284.600353] IPv6: ADDRCONF(NETDEV_CHANGE): eth1: link becomes ready

apalis_8qm:/ $ ifconfig eth0
eth0 Link encap:Ethernet HWaddr 00:14:2d:67:d5:03 Driver fec
inet addr:192.168.0.92 Bcast:192.168.0.255 Mask:255.255.255.0
inet6 addr: fe80::c7fe:c946:c301:ef9f/64 Scope: Link
UP BROADCAST RUNNING MULTICAST MTU:1500 Metric:1
RX packets:912 errors:0 dropped:0 overruns:0 frame:0
TX packets:52 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:1000
RX bytes:143444 TX bytes:5459

apalis_8qm:/ # ifconfig eth1
eth1 Link encap:Ethernet HWaddr 00:14:2d:77:d5:03 Driver fec
inet6 addr: fe80::214:2dff:fe77:d503/64 Scope: Link
UP BROADCAST RUNNING MULTICAST MTU:1500 Metric:1
RX packets:107 errors:0 dropped:0 overruns:0 frame:0
TX packets:9 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:1000
RX bytes:16389 TX bytes:746

apalis_8qm:/ # ping -I eth0 8.8.8.8
PING 8.8.8.8 (8.8.8.8) from 192.168.0.92 eth0: 56(84) bytes of data.
64 bytes from 8.8.8.8: icmp_seq=1 ttl=60 time=49.1 ms
64 bytes from 8.8.8.8: icmp_seq=2 ttl=60 time=48.8 ms
64 bytes from 8.8.8.8: icmp_seq=3 ttl=60 time=49.0 ms
64 bytes from 8.8.8.8: icmp_seq=4 ttl=60 time=48.7 ms

apalis_8qm:/ # ping -I eth1 8.8.8.8
ping: Warning: source address might be selected on device other than eth1.
PING 8.8.8.8 (8.8.8.8) from 0.0.0.0 eth1: 56(84) bytes of data.
From 127.0.0.1: icmp_seq=1 Destination Host Unreachable
From 127.0.0.1: icmp_seq=2 Destination Host Unreachable
From 127.0.0.1: icmp_seq=3 Destination Host Unreachable
From 127.0.0.1: icmp_seq=4 Destination Host Unreachable
From 127.0.0.1: icmp_seq=5 Destination Host Unreachable

I am using this dhcpcd set up in init.rc -

service dhcpcd_eth0 /system/bin/dhcpcd -ABKL eth0 eth1
class main
disabled
oneshot

service iprenew_eth0 /system/bin/dhcpcd -n eth0 eth1
class main
disabled
oneshot

Has anyone used both eth0 and eth1 with i.mx8 and Android 10?

Is the second ip address the issue?

Thank you.

0 Kudos
Reply
1 Solution
4,784 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Dear @SoftMicro You are welcome. Enjoy your vacation.

View solution in original post

0 Kudos
Reply
16 Replies
2,085 Views
FoxYang
Contributor I

Hi,

@Rita_Wang 

I have EthernetDual but it's some missing network interfaces to work with Android 13. I cannot get it to build yet. Some interfaces from NetworkUtils error.

Can you send me  EthernetDual(2).tar ?

Thanks.

0 Kudos
Reply
3,252 Views
spk
Contributor I

Hello @Rita_Wang ,
we are working on a custom board based on IMX8MP, where in we plan to use dual Ethernet on android 11. Could you please share me - 0001-android-device-nxp-dual-ethernet.patch and EthernetDual(2).tar

Thank you in advance.

 

0 Kudos
Reply
4,685 Views
sig0912
Contributor III

Hello @Rita_Wang , @SoftMicro 

I'm using imx8qm on custom board with Android 12 and I'm having the same issue where the host is unreachable when pinging from eth0 and eth1.
I could find the 0001-android-device-nxp-dual-ethernet.patch but I can't get the EthernetDual(2).tar

Could you please share this tarball?

Thank you!

0 Kudos
Reply
4,678 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

I share you by the email, please have a check.

0 Kudos
Reply
4,666 Views
sig0912
Contributor III

Thanks for sharing.

I just tried it but there are some missing network interfaces to work with Android 12. I cannot get it to build yet. Some interfaces from NetworkUtils are now deprecated for Android 12 and I'm now looking at the NetworkScore instead which seems to be the one to use.

I don't really do app like that so I'm a bit lost with the java files. Could you please explain what I should change to make EthernetDual package compatible with Android 12?

Thank you

0 Kudos
Reply
4,803 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

 I email to you, please have a check.

0 Kudos
Reply
4,797 Views
SoftMicro
Contributor II
I got your email with no content!
0 Kudos
Reply
4,794 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Have you got the 0001-android-device-nxp-dual-ethernet(4) and EthernetDual(2).tar I share to you?

0 Kudos
Reply
4,109 Views
chadA
Contributor III

Hi @Rita_Wang ,

Could you share these 2 packages with me?

Now I am also tring to use 2 ethernets on Imx8mm with android 9. And I am searching any useful information.

Thanks

Chad

0 Kudos
Reply
4,497 Views
vedantteksun
Contributor I
hI B45499, we are facing the same issue. Can I get these 2 files from you?
It will be very helpful.
0 Kudos
Reply
4,480 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Dear @vedantteksun ,

I email to you, please have a check. These patches are for the i.MX8MP, the method is the same, you can refer to.

Wish you have a nice day

Best Regards

Rita

0 Kudos
Reply
4,791 Views
SoftMicro
Contributor II
I can't access "NXP Office365 portal" to get these files. Can you email these directly or post here.

Thanks
0 Kudos
Reply
4,789 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

@SoftMicro This patch is for the i.MX8MP, for the i.MX8QM you can refer to

0 Kudos
Reply
4,786 Views
SoftMicro
Contributor II
Thank you so much b45499. I will try this out when I return from vacation in a week.
0 Kudos
Reply
4,785 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Dear @SoftMicro You are welcome. Enjoy your vacation.

0 Kudos
Reply
4,735 Views
SoftMicro
Contributor II
This fixed the issues, thank you