imx8 plus. Resolution 1920x1200 with two cameras

cancel
Showing results for 
Search instead for 
Did you mean: 

imx8 plus. Resolution 1920x1200 with two cameras

324 Views
Creative
Contributor III

Hi
Our iMX8 PLUS platform
We have two cameras daA3840-30mc

Can't get an image larger than 1920x1080. What needs to be changed in the kernel or driver to get a resolution of 1920x1280?

0 Kudos
2 Replies

307 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello Creative,

 

The i.MX8MP has a resolution maximum of 1920x1080, since is 1080p you cannot get more resolution since is the limit of hardware.

 

Regards

 

0 Kudos

283 Views
Creative
Contributor III

the documentation says that the maximum resolution is 1936x1188
How do we switch to this resolution 1936x1188?

0 Kudos