imx8: kirkstone yocto source image xen-minimal-image failing at do_rootfs

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

imx8: kirkstone yocto source image xen-minimal-image failing at do_rootfs

1,243 次查看
vsuneja63
Contributor III

Hi,

Thanks!

I am building xen-image-minimal on yocto kirkstone sources for imx8 EVK but its failing at rootfs with below error:

ERROR: xen-image-minimal-1.0-r0 do_rootfs: The postinstall intercept hook 'update_gtk_icon_cache' failed

Host machine: ubuntu 20.04

Any suggestion on this issue will be really helpful.

0 项奖励
回复
2 回复数

1,229 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

XEN only work on MX8QX and MX8QM, i think you are using MX8MQ.

 

Regards

 

0 项奖励
回复

1,225 次查看
vsuneja63
Contributor III

Hi,

Thanks!

I am building for imx8qm only, but this error doesn't seems to be specific to machine or EVK. Any suggestion on this issue?

Regards,

Vipul Kumar

 

0 项奖励
回复