imx8: kirkstone image not booting up if added systemd in local.conf

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx8: kirkstone image not booting up if added systemd in local.conf

1,003 Views
vsuneja63
Contributor III

Hi,

Thanks!

I am adding systemd in local.conf of kirkstone source to used systemctl. Image build successfully but it didn't ask for login password. Attaching a few last lines of logs, could see ip address also allocated but login is not coming up.

It boots up successfully if i remove systemd & build image. Not getting what is the exact issue while using systemd.

xhci_hcd 0000:01:00.0: xHCI Host Controller
xhci_hcd 0000:01:00.0: new USB bus registered, assigned bus number 1
xhci_hcd 0000:01:00.0: hcc params 0x002841eb hci version 0x100 quirks 0x0000040000000890
xhci_hcd 0000:01:00.0: xHCI Host Controller
xhci_hcd 0000:01:00.0: new USB bus registered, assigned bus number 2
xhci_hcd 0000:01:00.0: Host supports USB 3.0 SuperSpeed
hub 1-0:1.0: USB hub found
hub 1-0:1.0: 1 port detected
hub 2-0:1.0: USB hub found
hub 2-0:1.0: 4 ports detected
sdhci-iproc fe300000.mmc: allocated mmc-pwrseq
printk: console [netcon0] enabled
netconsole: network logging started
mmc0: SDHCI controller on fe300000.mmc [fe300000.mmc] using PIO
mmc1: SDHCI controller on fe340000.mmc [fe340000.mmc] using ADMA
md: Waiting for all devices to be available before autodetect
md: If you don't use raid, use raid=noautodetect
md: Autodetecting RAID arrays.
md: autorun ...
md: ... autorun DONE.
Waiting for root device PARTUUID=bbea8a01-02...
mmc1: new ultra high speed DDR50 SDHC card at address aaaa
mmcblk1: mmc1:aaaa SD32G 29.7 GiB
mmc0: new high speed SDIO card at address 0001
mmcblk1: p1 p2
EXT4-fs (mmcblk1p2): mounting ext3 file system using the ext4 subsystem
EXT4-fs (mmcblk1p2): INFO: recovery required on readonly filesystem
EXT4-fs (mmcblk1p2): write access will be enabled during recovery
EXT4-fs (mmcblk1p2): recovery complete
EXT4-fs (mmcblk1p2): mounted filesystem with ordered data mode. Opts: (null). Quota mode: disabled.
VFS: Mounted root (ext3 filesystem) readonly on device 179:2.
devtmpfs: mounted
Freeing unused kernel memory: 4224K
usb 1-1: new high-speed USB device number 2 using xhci_hcd
Run /sbin/init as init process
with arguments:
/sbin/init
with environment:
HOME=/
TERM=linux
INIT: version 3.01 booting
hub 1-1:1.0: USB hub found
hub 1-1:1.0: 4 ports detected
fbcon: Taking over console
Console: switching to colour frame buffer device 228x61
Starting udev
/etc/rcS.d/S03systemd-udevd: line 76: /proc/sys/kernel/hotplug: No such file or directory
usb 1-1.3: new low-speed USB device number 3 using xhci_hcd
Starting version 250.5+
input: PixArt Dell MS116 USB Optical Mouse as /devices/platform/scb/fd500000.pcie/pci0000:00/0000:00:00.0/0000:01:00.0/usb1/1-1/1-1.3/1-1.3:1.0/0003:413C:301A.0001/input/input0
hid-generic 0003:413C:301A.0001: input: USB HID v1.11 Mouse [PixArt Dell MS116 USB Optical Mouse] on usb-0000:01:00.0-1.3/input0
EXT4-fs (mmcblk1p2): re-mounted. Opts: (null). Quota mode: disabled.
Fri Mar 9 12:34:56 UTC 2018
INIT: Entering runlevel: 5
Configuring network interfaces... udhcpc: started, v1.35.0
bcmgenet fd580000.ethernet: configuring instance for external RGMII (RX delay)
bcmgenet fd580000.ethernet eth0: Link is Down
udhcpc: broadcasting discover
bcmgenet fd580000.ethernet eth0: Link is Up - 1Gbps/Full - flow control off
udhcpc: broadcasting discover
IPv6: ADDRCONF(NETDEV_CHANGE): eth0: link becomes ready
udhcpc: broadcasting discover
udhcpc: broadcasting select for 192.168.1.39, server 192.168.1.1
udhcpc: lease of 192.168.1.39 obtained from 192.168.1.1, lease time 86400
/etc/udhcpc.d/50default: Adding DNS 192.168.1.1
done.
Starting system message bus: dbus.
Starting random number generator daemon.
Starting OpenBSD Secure Shell server: sshd
done.
Starting syslogd/klogd: done
Starting domain watchdog daemon: [ OK ]

Any suggestion on this will be really helpful.

Labels (1)
0 Kudos
Reply
0 Replies