imx8: gdb-cross-canadian do_compile failed while building toolchain

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

imx8: gdb-cross-canadian do_compile failed while building toolchain

2,633 次查看
vsuneja63
Contributor III

Hi,

Building toolchain for bsp 5.4, facing gdb-cross-Canadian error. Building image on host ubuntu16.04. Here are the logs: 

ERROR: gdb-cross-canadian-aarch64-9.1-r0 do_compile: oe_runmake failed
ERROR: gdb-cross-canadian-aarch64-9.1-r0 do_compile: Execution of '/home/vipulkumar/platform/AGL_Jellyfish/build/tmp/work/x86_64-nativesdk-aglsdk-linux/gdb-cross-canadian-aarch64/9.1-r0/temp/run.do_compile.6025' failed with exit code 1:
make: *** No targets specified and no makefile found.  Stop.
WARNING: exit code 1 from a shell command.

ERROR: Logfile of failure stored in: /home/vipulkumar/platform/AGL_Jellyfish/build/tmp/work/x86_64-nativesdk-aglsdk-linux/gdb-cross-canadian-aarch64/9.1-r0/temp/log.do_compile.6025
Log data follows:
| DEBUG: Executing python function autotools_aclocals
| DEBUG: SITE files ['endian-little', 'common-linux', 'common-glibc', 'bit-64', 'x86_64-linux', 'common']
| DEBUG: Python function autotools_aclocals finished
| DEBUG: Executing shell function do_compile
| NOTE: make -j 8 SUBDIRS=intl mmalloc libiberty opcodes bfd sim gdb etc utils
| make: *** No targets specified and no makefile found.  Stop.
| ERROR: oe_runmake failed
| WARNING: exit code 1 from a shell command.
| ERROR: Execution of '/home/vipulkumar/platform/AGL_Jellyfish/build/tmp/work/x86_64-nativesdk-aglsdk-linux/gdb-cross-canadian-aarch64/9.1-r0/temp/run.do_compile.6025' failed with exit code 1:
| make: *** No targets specified and no makefile found.  Stop.
| WARNING: exit code 1 from a shell command.
|
ERROR: Task (/home/vipulkumar/platform/AGL_Jellyfish/external/poky/meta/recipes-devtools/gdb/gdb-cross-canadian_9.1.bb:do_compile) failed with exit code '1'

标签 (1)
0 项奖励
回复
3 回复数

2,589 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport
0 项奖励
回复

2,578 次查看
vsuneja63
Contributor III

Hi,

Thanks!

I couldn't get patches on the given links, can you please share something specific on the same? packagegroup-cross-canadian.bb source file is same only.

0 项奖励
回复

2,616 次查看
vsuneja63
Contributor III

Hi!

Any suggestion on the issue?

0 项奖励
回复