I used imx8mq, android 9.0.In the uboot, I use fastboot 0 to enter the fastboot mode, and I can use the UUU tool to download the firmware.However, in the Windows CMD environment, using fastboot devices does not see any devices.Normal boot on android, same with adb reboot bootloader.
Is it because the fastboot in android 9.0 only supports UUU devices and cannot use adb/fastboot tools?
It is a known fact that updating FW using Fastboot fails in WIN10. We expect the NXP R&D team to solve this problem and provide a suitable fastboot USB driver for win10. After all, factories and ordinary people install Windows 10.
https://community.nxp.com/t5/i-MX-Processors/MX8MM-won-t-enter-fastboot-mode/m-p/937720#M140466 <- NO WORK!!!
However this is a very serious problem!!!
Hello,
Sometimes the host PC selects an incorrect driver model of the USB devices, leading to the PC inability to find fastboot devices, please follow this steps
1.- Run "reboot bootloader" in console after boot (device side)
2.- in host side, open "Computer Management->Device Manager", you'll note that the USB appears as:
Universal Serial Bus devices -> USB download gadget
3.- Right click it, and choose “Updated Driver -> browse my computer for driver software -> let me pick from a list of available drivers on my computer”, clear “Show compatible hardware” item, then choose “ADB devices”.
4.-Select yes to the pop-up window, this will select the USB as an ADB device.
Reboot your device and it should be listed on your host for adb/fastboot tools
Hope this helps,
Best regards,
Aldo.
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Hi,
I am also facing same issue. Is it resolved for you?.