imx8 ddr config

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx8 ddr config

1,255 Views
gravity_one
Contributor III

Hello, All

TOOLS:

   MX8QXP_C0_B0_LPDDR4_RPA_1.2GHz_v13.xlsx

   mx8_ddr_stress_test_ER14_installation.zip

BOARD: Imx8qxp mek  DDR stress test

   LPDDR4 3G  --->4G

test log:

*************************************************************************
MX8 DDR Stress Test Version: ER14
Built on Mar 27 2020 12:28:23
*************************************************************************

-Set up the MMU and enable I and D cache-

  • This is the Cortex-A35 core
  • Check if I cache is enabled
  • Enabling I cache since it was disabled
  • Push base address of TTB to TTBR0_EL3
  • Config TCR_EL3
  • Config MAIR_EL3
  • Enable MMU
  • Data Cache has been enabled
  • Check system memory register, only for debug
  • VMCR Check:
  • ttbr0_el3: 0x13d000
  • tcr_el3: 0x2051c
  • mair_el3: 0x774400
  • sctlr_el3: 0xc01815
  • id_aa64mmfr0_el1: 0x101122
  • MMU and cache setup complete

*************************************************************************
ARM Clock(CA35): 1200MHz
DDR Clock: 1200MHz

============================================
DDR configuration
DDR type is LPDDR4
Data width: 32, bank num: 8
Row size: 16, col size: 10
Two chip selects are used
Number of DDR controllers used on the SoC: 1
Density per chip select: 2048MB
Density per controller is: 4096MB
Total density detected on the board is: 4096MB

No DDR data training errors detected for DDRC0
============================================

MX8QXP: Cortex-A35 is found

*************************************************************************
DDR Stress Test Iteration 1
--------------------------------
-Running DDR test on region 1-
--------------------------------

t0.1: data is addr test
....
t0.2: row hop read test
...

t1: memcpy SSN armv8_x32 test
....
t2: byte-wise SSN armv8_x32 test
..
t3: memcpy pseudo random pattern test
....................................................................
t4: IRAM_to_DDRv1 test
...

t5: IRAM_to_DDRv2 test
--------------------------------
-Running DDR test on region2-
--------------------------------

t0.1: data is addr 

(Stuck here, didn't know it was wrong, stayed there for 20 minutes, restarted the test many times and still did the same thing)

0 Kudos
3 Replies

1,210 Views
igorpadykov
NXP Employee
NXP Employee

Hi Wang

one can recheck "BoardDataBusConfig" settings in RPA tool and

tweak drive strength settings.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

1,210 Views
gravity_one
Contributor III

hello, igor

I don't know why I pressed the download button of the case. Now it is shown in the picture, and there is no other display

pastedImage_1.png

tks

0 Kudos

1,210 Views
gravity_one
Contributor III

hello, igor

can you tell me how to setting "BoardDataBusConfig"?

only modify

Density per channel per chip select (Gb)1:6

to 8.

tks

0 Kudos