imx8: couldn't launch h264 gstreamer pipeline after killing gstreamer multiple times.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx8: couldn't launch h264 gstreamer pipeline after killing gstreamer multiple times.

2,816件の閲覧回数
ondrejbilka
Contributor II

When one repeatedly launches gstreamer using h264 vpudec and then terminating it with killall it leads to situation where pipeline stops working. From log below it looks like that it doesn't properly free decoder and they run out. I couldn't replicate this behaviour by using gst-launch -e and properly termination it with ctrl-c sending EOS.

gst-launch-1.0: ../../source/h264high/h264hwd_asic.c:1009: H264RunAsic: Assertio
n `0' failed.
test: line 10: 5842 Aborted (core dumped) gst-launch-1.0 -e -v
$START vpudec ! textoverlay text="blabla" ! $SINK

[ 505.839740] audit: type=1701 audit(1520332016.986:12): auid=4294967295 uid=0 gid=0 ses=4294967295 pid=5284 comm="rtpjitterbuffer" exe="/usr/bin/gst-launch-1.0" sig=6
[ 510.376891] hantrodec: DEC[0] still enabled -> reset
[ 510.417429] hantrodec: DEC[0] still enabled -> reset
[ 510.435842] hantrodec: DEC[0] still enabled -> reset

As side note how one builds h264 encoder? It could lead to easier example of videotestsrc ! encode h264 ! vpudec ! glimagesink

test scripts are

test: 

gst-launch-1.0 ...(rtsp h264 stream from camera) ! vpudec ! glimagesink

runtest:

for ì in `seq 1 100`; do

sh test &

sleep 3

killall gst-launch-1.0

done

ラベル(4)
タグ(1)
0 件の賞賛
返信
3 返答(返信)

2,178件の閲覧回数
ondrejbilka
Contributor II

Ping,

I mostly want to know status, if somebody is looking into this or not?

Or if bugs should be reported in different system?

2,178件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

why would you stop the gstreamer again and again? it seems killall command doesn't release the memory, I don't know if we can use other option, could you tell me what's your demands of your case?

0 件の賞賛
返信

2,178件の閲覧回数
ondrejbilka
Contributor II

Mainly this should be at least documented.

As QA issue it means that one must put gstreamer parts into separate process to minimize risk of crash.

This means that one couldn't with not very important application like displaying weather that uses lot of third party code and gstreamer relaunch it when it crashes. It would cause more important applications failure after weather one crashes enough times.

0 件の賞賛
返信