imx8: couldn't launch h264 gstreamer pipeline after killing gstreamer multiple times.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx8: couldn't launch h264 gstreamer pipeline after killing gstreamer multiple times.

1,616 Views
ondrejbilka
Contributor II

When one repeatedly launches gstreamer using h264 vpudec and then terminating it with killall it leads to situation where pipeline stops working. From log below it looks like that it doesn't properly free decoder and they run out. I couldn't replicate this behaviour by using gst-launch -e and properly termination it with ctrl-c sending EOS.

gst-launch-1.0: ../../source/h264high/h264hwd_asic.c:1009: H264RunAsic: Assertio
n `0' failed.
test: line 10: 5842 Aborted (core dumped) gst-launch-1.0 -e -v
$START vpudec ! textoverlay text="blabla" ! $SINK

[ 505.839740] audit: type=1701 audit(1520332016.986:12): auid=4294967295 uid=0 gid=0 ses=4294967295 pid=5284 comm="rtpjitterbuffer" exe="/usr/bin/gst-launch-1.0" sig=6
[ 510.376891] hantrodec: DEC[0] still enabled -> reset
[ 510.417429] hantrodec: DEC[0] still enabled -> reset
[ 510.435842] hantrodec: DEC[0] still enabled -> reset

As side note how one builds h264 encoder? It could lead to easier example of videotestsrc ! encode h264 ! vpudec ! glimagesink

test scripts are

test: 

gst-launch-1.0 ...(rtsp h264 stream from camera) ! vpudec ! glimagesink

runtest:

for ì in `seq 1 100`; do

sh test &

sleep 3

killall gst-launch-1.0

done

Tags (1)
0 Kudos
3 Replies

978 Views
ondrejbilka
Contributor II

Ping,

I mostly want to know status, if somebody is looking into this or not?

Or if bugs should be reported in different system?

978 Views
joanxie
NXP TechSupport
NXP TechSupport

why would you stop the gstreamer again and again? it seems killall command doesn't release the memory, I don't know if we can use other option, could you tell me what's your demands of your case?

0 Kudos

978 Views
ondrejbilka
Contributor II

Mainly this should be at least documented.

As QA issue it means that one must put gstreamer parts into separate process to minimize risk of crash.

This means that one couldn't with not very important application like displaying weather that uses lot of third party code and gstreamer relaunch it when it crashes. It would cause more important applications failure after weather one crashes enough times.

0 Kudos