Hi,
Thanks!
imx8mq-evk connected with Android mobile via Bluetooth. Audio streaming happening from android to imx8mq-evk. Could hear music on 3.5mm jack but intermediate noise is also there. Trying to remove the noise, trying to attach device with baud rate but its failing.
Used hciattach command: "hciattach /dev/ttymxc2 qualcomm"
Trying to add baud rate with command but its failing, here is the command: "hciattach /dev/ttymxc2 qualcomm 3000000"
logs:
imx8mqevk:/home# hciattach /dev/ttymxc2 qualcomm 3000000
Qualcomm module LMP version : 0x07
Qualcomm module LMP sub-version : 0x025a
Opening firmware file: /etc/firmware/6.03.0_0602.bin
Could not open firmware file /etc/firmware/6.03.0_0602.bin: No such file or directory (2).
Setting TTY to N_HCI line discipline
Can you suggest solution for removing noise or anything on baud rate issue?
Target: imx8mq-evk
BSP: 5.4
Host: ubuntu16.04
Hi,
Thanks!
Its a blocking point for me. Any suggestion on the issue could be helpful.
Hi vsuneja63
there are several android releases with "BSP: 5.4", may be recommended to try
latest ones (please read Release Notes document which particular bluetooth chip is supported)
Best regards
igor