imx8: bluetooth audio streaming to imx8mq-evk output has intermediate noise

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx8: bluetooth audio streaming to imx8mq-evk output has intermediate noise

1,581 Views
vsuneja63
Contributor III

Hi,

Thanks!

imx8mq-evk connected with Android mobile via Bluetooth. Audio streaming happening from android to imx8mq-evk. Could hear music on 3.5mm jack but intermediate noise is also there. Trying to remove the noise, trying to attach device with baud rate but its failing.

Used hciattach command: "hciattach /dev/ttymxc2 qualcomm"

Trying to add baud rate with command but its failing, here is the command: "hciattach /dev/ttymxc2 qualcomm 3000000"

logs:

imx8mqevk:/home# hciattach /dev/ttymxc2 qualcomm 3000000
Qualcomm module LMP version : 0x07
Qualcomm module LMP sub-version : 0x025a
Opening firmware file: /etc/firmware/6.03.0_0602.bin
Could not open firmware file /etc/firmware/6.03.0_0602.bin: No such file or directory (2).
Setting TTY to N_HCI line discipline

Can you suggest solution for removing noise or anything on baud rate issue?

Target: imx8mq-evk

BSP: 5.4

Host: ubuntu16.04

Labels (1)
0 Kudos
Reply
2 Replies

1,569 Views
vsuneja63
Contributor III

Hi,

Thanks!

Its a blocking point for me. Any suggestion on the issue could be helpful.

0 Kudos
Reply

1,549 Views
igorpadykov
NXP Employee
NXP Employee

Hi vsuneja63

 

there are several android releases with "BSP: 5.4", may be recommended to try

latest ones (please read Release Notes document which particular bluetooth chip is supported)

 

https://www.nxp.com/design/software/embedded-software/i-mx-software/android-os-for-i-mx-applications...

 

Best regards
igor

0 Kudos
Reply