hi,
I use systemctl stop weston@root.service cmd,stop weston service.
then,
/unit_tests/V4L2/mx8_v4l2_cap_drm.out -cam 1 -d "/dev/video1" -fmt UYVY
can Display the camera screen,
but,Cannot display normally when using QT application。It seems that under wayland, video data cannot be read normally。The version of L5.4.47 is relatively new, can you give me some help.
Thanks
tried the "qmlglsrccamera", "test_qmlglsink", "test_qmlglsrc" under path "/usr/share/qt5/examples/multimedia/qmlgltest", and they are all OK to display on the Weston, with LVDS to HDMI output.I used xwayland
HI,
I mean "qmlglsrccamera", "test_qmlglsink", "test_qmlglsrc" , source code,
I am not very familiar with gstreamer yet, I need to refer to some
HI,
I can not find the source code ,can you tell me the source code location,in yocto project.
I compile imx-image-full,L5.4.47
Thanks,
after building, you need download images to the board, you can find it after board boot up
HI,
I know,I found these files in the directory of the board, but I want to find the corresponding source code
Thanks
maybe you can refer to the source code from path:
"/imx-yocto-bsp/build-xwayland/tmp/work/aarch64-poky-linux/qtmultimedia/5.15.0+gitAUTOINC+040378a91f-r0/git/examples/multimedia/"
HI,
I just came into contact with gst-launch-1.0,can you give a cmd,to playing the /dev/videox .
the /dev/videox is v4l, lvds screen
Thanks
HI,
Found it,thank you very much!
Thanks!
Hello,
Were you ever able to find the source code for this example? I have only been able to find the binaries myself.
Thanks!
- Graham