imx8 MIPS GFLOP?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx8 MIPS GFLOP?

4,396 Views
baijinlong
Contributor III

We are currently evaluating the performance of the imx8 family of processors. We found the CPU and GPU performance parameters for imx8 and imx8m, but for the imx8x and imx8m mini series, we were unable to find the relevant parameters.

E.g:

 i.MX 8QuadMaxi.MX 8QuadPlusi.MX 8DualMax
CPU 2xA72+4xA531xA72+4xA532xA72
DMIPS26k18.5k15k
GPU2x GC7000 XSVX2x GC7000Lite XSVX1x GC7000 XSVX
GFLOPS1288064
 i.MX 8MQuadi.MX 8MQuadLitei.MX 8Dual
CPU 4xA534xA532xA53
DMIPS13.8k13.8k6.9k
GPUGC7000LiteGC7000LiteGC7000Lite
GFLOPS646464

1. What is the DMIPS of the CPU of the imx8x (8qxp, 8dxp, 8dx) series, and what is the GFLOP of the GPU?
2. What is the DMIPS of the CPU of the imx8m mini (Mini Quad, Mini Dual, Mini Solo) series, and what is the GFLOP of the GPU?

0 Kudos
Reply
1 Reply

3,504 Views
CarlosCasillas
NXP Employee
NXP Employee

Hi Jinlong,

Unfortunately, we do not have any performance data that we can share, please contact your NXP Sales/FAE regarding these features, they would be able to help you.


Hope this will be useful for you.
Best regards!
/Carlos
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
-------------------------------------------------------------------------------

0 Kudos
Reply