imx8: Building "xen-image-minimal" failing on rootfs for imx8mqevk target

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx8: Building "xen-image-minimal" failing on rootfs for imx8mqevk target

2,209 Views
vsuneja63
Contributor III

I am trying to build xen hypervisor for imx8mqevk target by command "bitbake xen-image-minimal" but its failing at do_rootfs.

ERROR: xen-image-minimal-1.0-r0 do_rootfs: Could not invoke dnf. Command '/home/vipulkumar/platform/AGL_Master/build/tmp/work/imx8mqevk-agl-linux/xen-image-minimal/1.0-r0/recipe-sysroot-native/usr/bin/dnf -v --rpmverbosity=debug -y -c /home/vipulkumar/platform/AGL_Master/build/tmp/work/imx8mqevk-agl-linux/xen-image-minimal/1.0-r0/rootfs/etc/dnf/dnf.conf --setopt=reposdir=/home/vipulkumar/platform/AGL_Master/build/tmp/work/imx8mqevk-agl-linux/xen-image-minimal/1.0-r0/rootfs/etc/yum.repos.d --repofrompath=oe-repo,/home/vipulkumar/platform/AGL_Master/build/tmp/work/imx8mqevk-agl-linux/xen-image-minimal/1.0-r0/oe-rootfs-repo --installroot=/home/vipulkumar/platform/AGL_Master/build/tmp/work/imx8mqevk-agl-linux/xen-image-minimal/1.0-r0/rootfs --setopt=logdir=/home/vipulkumar/platform/AGL_Master/build/tmp/work/imx8mqevk-agl-linux/xen-image-minimal/1.0-r0/temp --nogpgcheck install locale-base-en-us locale-base-en-gb kernel-modules kernel-module-xen-gntalloc packagegroup-core-standalone-sdk-target pulseaudio-server rpm packagegroup-core-tools-debug dropbear sdl-core kernel-module-xen-netback screen kernel-module-xen-blkback packagegroup-core-tools-profile kernel-module-xen-gntdev libdrm-tests xen-base kernel-module-xen-wdt dnf mc run-postinsts packagegroup-core-boot packagegroup-agl-core-devel packagegroup-core-sdk libz-dev qemu packagegroup-core-eclipse-debug packagegroup-core-ssh-openssh busybox' returned 1:
DNF version: 2.7.5
cachedir: /home/vipulkumar/platform/AGL_Master/build/tmp/work/imx8mqevk-agl-linux/xen-image-minimal/1.0-r0/rootfs/var/cache/dnf
Added oe-repo repo from /home/vipulkumar/platform/AGL_Master/build/tmp/work/imx8mqevk-agl-linux/xen-image-minimal/1.0-r0/oe-rootfs-repo
repo: using cache for: oe-repo
not found deltainfo for: oe-repo
not found updateinfo for: oe-repo
oe-repo: using metadata from Tue 10 Mar 2020 11:11:03 AM UTC.
Last metadata expiration check: 0:00:02 ago on Tue 10 Mar 2020 11:11:11 AM UTC.
No match for argument: kernel-module-xen-gntalloc
No match for argument: kernel-module-xen-blkback
No match for argument: kernel-module-xen-gntdev
No match for argument: kernel-module-xen-wdt
Error: Unable to find a match

0 Kudos
Reply
5 Replies

2,069 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello Vipul,

 

The error says it can't find a package named repo. Was such a package generated? For this error I strongly recommend to erase and reinstall the yocto again. Or maybe you are playing with non-supported ubuntu version.

 

Regards

0 Kudos
Reply

2,070 Views
vsuneja63
Contributor III

Hi,

Thanks for reply!

 

I am building xen hypervisor for imx8mq target. Does xen support imx8mq ?

If support is available how i can find device tree source for the same, xen supporting dts files are available for imx8qm & imx8qxp only.

kernel: 4.19.35

u-boot: 2019.04

host: ubuntu 16.04

Looking forward for your response.

 

Thanks & Regards,

Vipul Kumar

0 Kudos
Reply

2,070 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

Xen is not supported in MX8MQ, still working on it,  but it will be supported in at least two more BSP.

Regards

0 Kudos
Reply

2,070 Views
vsuneja63
Contributor III

Hi,

Any suggestion on the supporting hypervisor. Is there any timeline specified for Xen support on imx8mq?

Would like to hear from you.

Thanks & Regards,

Vipul Kumar

0 Kudos
Reply

2,070 Views
vsuneja63
Contributor III

Hi,

Thanks for reply!

I am trying to load yocto based linux OS in each core of imx8mq EVK. OS in each core should be isolated. Can you suggest which hypervisor can serve my purpose?

I tried jailhouse but looks like it only support RTOS in non-root cells & as you mention Xen doesn't support imx8mq. Looking forward to hear from you on this.  

Thanks & Regards,

Vipul Kumar

0 Kudos
Reply