Hi,
We're using the latest recommended FSL Yocto release ( document NXP Rev. L4.9.88_2.0.0-ga, 05/2018 ) Rocko ( kernel 4.9.88 ) on a custom iMx7d board and are getting an error -16 when probing usdhc2 ( esdhc controller 30b50000 )
This board is a known working board, eMMC works on usdhc3, 1DX BT/WiFi module on usdhc1 and the sd card slot on usdhc2. If we use the Krogoth 4.1 kernel then everything works fine; but the kernel is too old for our requirements.
Using the newer 4.9.88 BSP the sd-card slot usdhc2 fails on probing ( eMMC works fine ). The device tree changes are very basic and are tried and tested on the earlier 4.1 kernel. Same failure if booted with card in or out.
[ 2nd sd-card slot settings, fine on 4.1 kernel, fails on 4.9.88 kernel ]
&usdhc2 {
pinctrl-names = "default", "state_100mhz", "state_200mhz";
pinctrl-0 = <&pinctrl_usdhc2>;
pinctrl-1 = <&pinctrl_usdhc2_100mhz>;
pinctrl-2 = <&pinctrl_usdhc2_200mhz>;
/* MX7D_PAD_SD2_CD_B__GPIO5_IO9 */
cd-gpios = <&gpio5 9 GPIO_ACTIVE_LOW>;
/* MX7D_PAD_SD2_WP__GPIO5_IO10 */
wp-gpios = <&gpio5 10 GPIO_ACTIVE_HIGH>;
bus-width = <4>;
removable;
wakeup-source;
// vmmc-supply = <®_sd1_vmmc>;
enable-sdio-wakeup;
keep-power-in-suspend;
status = "okay";
};
Booting with kernel sdhc debug on offers no extra insight; I get the following:
sdhci: Secure Digital Host Controller Interface driver
sdhci: Copyright(c) Pierre Ossman
usbcore: registered new interface driver ushc
sdhci-pltfm: SDHCI platform and OF driver helper
sdhci-esdhc-imx: probe of 30b50000.usdhc failed with error -16 <== 2nd sd card slot fails
mmc0: SDHCI controller on 30b60000.usdhc [30b60000.usdhc] using ADMA <== eMMC good
One forum mentioned an aliases { mmc2 = &usdhc2; } problem with 4.9 kernels but this didn't do anything, bear in mind the eMMC is found on usdhc3 alright...
To summarize; known board, dtb settings work with 4.1 kernel but fail when used with the 4.9.88 kernel.
Thanks.
已解决! 转到解答。