imx7d - second ethernet port is not working with kernel 4.9.39

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

imx7d - second ethernet port is not working with kernel 4.9.39

3,544 次查看
vinothkumareswa
Contributor II

Hello,

I am working on a compulab board -

CL-SOM-iMX7 | NXP (Freescale) i.MX 7 | System-on-Module | Computer-on-Module | CompuLab .

Currently I am trying to build the latest LTS kernel version for the board - Linux 4.9.39. I have added the necessary device tree changes. In imx7d.dtsi file which includes imx7s.dtsi, I could see that only one ethernet device (fec1) is added. So I have added the second ethernet device as in old dtsi files under aips3 section,

    fec2: ethernet@30bf0000 {
        compatible = "fsl,imx7d-fec", "fsl,imx6sx-fec";
        reg = <0x30bf0000 0x10000>;
        interrupts = <GIC_SPI 100 IRQ_TYPE_LEVEL_HIGH>,
            <GIC_SPI 101 IRQ_TYPE_LEVEL_HIGH>,
            <GIC_SPI 102 IRQ_TYPE_LEVEL_HIGH>;
        clocks = <&clks IMX7D_ENET_AXI_ROOT_CLK>,
            <&clks IMX7D_ENET_AXI_ROOT_CLK>,
            <&clks IMX7D_ENET2_TIME_ROOT_CLK>,
            <&clks IMX7D_PLL_ENET_MAIN_125M_CLK>,
            <&clks IMX7D_ENET_PHY_REF_ROOT_CLK>;
        clock-names = "ipg", "ahb", "ptp",
            "enet_clk_ref", "enet_out";
        stop-mode = <&gpr 0x10 4>;
        fsl,num-tx-queues=<3>;
        fsl,num-rx-queues=<3>;
        fsl,wakeup_irq = <2>;
        status = "disabled";
    };

In my device tree file I have enabled the ethernet device by the following configuration:

&fec1 {
    pinctrl-names = "default";
    pinctrl-0 = <&pinctrl_enet1>;
    depends = "/soc/aips-bus@30800000/i2c@30a30000/pca9555@20";
    pinctrl-assert-gpios = <&gpio1 4 GPIO_ACTIVE_HIGH> , <&pca9555 4 GPIO_ACTIVE_HIGH>;
    assigned-clocks = <&clks IMX7D_ENET1_TIME_ROOT_SRC>,
              <&clks IMX7D_ENET1_TIME_ROOT_CLK>;
    assigned-clock-parents = <&clks IMX7D_PLL_ENET_MAIN_100M_CLK>;
    assigned-clock-rates = <0>, <100000000>;
    phy-mode = "rgmii";
    phy-handle = <&ethphy0>;
    fsl,magic-packet;
    status = "okay";

    mdio {
        #address-cells = <1>;
        #size-cells = <0>;

        ethphy0: ethernet-phy@0 {
            compatible = "ethernet-phy-ieee802.3-c22";
            reg = <0>;
        };

        ethphy1: ethernet-phy@1 {
            compatible = "ethernet-phy-ieee802.3-c22";
            reg = <1>;
        };
    };
};

&fec2 {
    pinctrl-names = "default";
    pinctrl-0 = <&pinctrl_enet2>;
    assigned-clocks = <&clks IMX7D_ENET2_TIME_ROOT_SRC>,
              <&clks IMX7D_ENET2_TIME_ROOT_CLK>;
    assigned-clock-parents = <&clks IMX7D_PLL_ENET_MAIN_100M_CLK>;
    assigned-clock-rates = <0>, <100000000>;
    phy-mode = "rgmii";
    phy-handle = <&ethphy1>;
    fsl,magic-packet;
    status = "okay";
};

I have builded the Linux kernel using Yocto (Pyro). After booting the device only eth0 is working fine, the second ethernet (eth1) port is  not working. After connecting the cable no lights are flashing and also the link is not coming up.

ifconfig shows only eth0 as shown below:

root@alen-iot-gateway:~# ifconfig
eth0      Link encap:Ethernet  HWaddr 00:01:C0:1E:36:B1  
          UP BROADCAST MULTICAST  MTU:1500  Metric:1
          RX packets:0 errors:0 dropped:0 overruns:0 frame:0
          TX packets:0 errors:0 dropped:0 overruns:0 carrier:0
          collisions:0 txqueuelen:1000
          RX bytes:0 (0.0 B)  TX bytes:0 (0.0 B)

lo        Link encap:Local Loopback  
           inet addr:127.0.0.1  Mask:255.0.0.0

ifconfig -a shows both devices as shown below:

root@alen-iot-gateway:~# ifconfig -a

eth0      Link encap:Ethernet  HWaddr 00:01:C0:1E:36:B1  
          UP BROADCAST MULTICAST  MTU:1500  Metric:1
          RX packets:0 errors:0 dropped:0 overruns:0 frame:0
          TX packets:0 errors:0 dropped:0 overruns:0 carrier:0
          collisions:0 txqueuelen:1000
          RX bytes:0 (0.0 B)  TX bytes:0 (0.0 B)

eth1      Link encap:Ethernet  HWaddr 3A:00:FC:9E:6B:4F  
          BROADCAST MULTICAST  MTU:1500  Metric:1
          RX packets:0 errors:0 dropped:0 overruns:0 frame:0
          TX packets:0 errors:0 dropped:0 overruns:0 carrier:0
          collisions:0 txqueuelen:1000
           RX bytes:0 (0.0 B)  TX bytes:0 (0.0 B)

When I tried to run 'ifconfig eth1 up'  i get the following error message:

root@alen-iot-gateway:~# ifconfig eth1 up
ifconfig: SIOCSIFFLAGS: No such device
root@alen-iot-gateway:~# ifconfig eth1 down
root@alen-iot-gateway:~# ifconfig eth1 up
ifconfig: SIOCSIFFLAGS: No such device

with ethtool I get the following error messages,

root@alen-iot-gateway:~# ethtool eth1
Settings for eth1:
Cannot get device settings: No such device
        Supports Wake-on: g
        Wake-on: d
        Link detected: no

The dmesg for ethernet is shown below:

dmesg | grep -i eth
Atheros(R) L2 Ethernet Driver - version 2.2.3
30be0000.ethernet supply phy not found, using dummy regulator
fec 30be0000.ethernet eth0: registered PHC device 0
30bf0000.ethernet supply phy not found, using dummy regulator
fec 30bf0000.ethernet (unnamed net_device) (uninitialized): Invalid MAC address: 00:00:00:00:00:00
fec 30bf0000.ethernet (unnamed net_device) (uninitialized): Using random MAC address: 3a:00:fc:9e:6b:4f
fec 30bf0000.ethernet eth1: registered PHC device 1
Bluetooth: BNEP (Ethernet Emulation) ver 1.3
Atheros 8031 ethernet 30be0000.etherne:00: attached PHY driver [Atheros 8031 ethernet] (mii_bus:phy_addr=30be0000.etherne:00, irq=-1)
IPv6: ADDRCONF(NETDEV_UP): eth0: link is not ready
fec 30be0000.ethernet eth0: Link is Up - 1Gbps/Full - flow control rx/tx
IPv6: ADDRCONF(NETDEV_CHANGE): eth0: link becomes ready

Not sure on what configuration is missing for the ethernet port. Any information on the topic would be helpful. Let me know if any further logs are required

Thanks & Regards,

Vinothkumar

标签 (3)
0 项奖励
回复
3 回复数

2,222 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Vinothkumar

for second port configuration one can look at imx7d-12x12-lpddr3-arm2-enet2.dts

linux-imx.git - i.MX Linux Kernel 

try with offical nxp bsps described on

http://www.nxp.com/products/software-and-tools/software-development-tools/i.mx-software-and-tools/i....

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

2,223 次查看
vinothkumareswa
Contributor II

Hi Igor,

Currently I am using the Kernel from NXP repo(imx_4.1.15_1.0.0_ga)

          git://git.freescale.com/imx/linux-2.6-imx.git. Kernel version:4.1.15

My idea is to use the latest kernel. On the NXP repositories I didn't find any kernel version later than 4.1.15.

Regards,

Vinoth

0 项奖励
回复

2,223 次查看
lakshmishetty
Contributor II

Hi Vinothkumar,

Even I am facing the same issue(second ethernet is not working).  Have you fixed that issue. If so, could you please suggest how to fix it.

Thanks,

Best Regards,
Lakshmi  Shetty

0 项奖励
回复