Hello everyone
my development board is IMX7DSABRE. Linux kernel version is 4.9.88
When I use SPI to transfer data on imx7d, my imx7d is the master device and my module is the slave device. My module receives 32bit data at a time. The driver I use is driver/spi/spidev.c. The test program I use is tools/spi/spidev_test.c.
If I transmit 8bit data each time, then there will be no problem, but if I transmit 32bit data each time, the program prompts: can't send spi message: Invalid argument
How can I transfer 32-bit data at a time.
By the way, I have achieved 16-bit half-duplex transmission through the read and write functions. But our SPI must work in full-duplex mode, that is, to use the spidev_message function area to transfer data.
Excuse me, how should I solve the problem I am facing now?
Hi Qidong,
See below, please!
----------------------------
1.The communication mode of SPI is originally full-duplex communication.
2. SPI allows 8bit and 16bit data transmission.
3. If you use 8bit mode, you need to send 4 times in a loop to achieve the purpose of transmitting 32bit data.
-----------------------------
Hope the information is helpful to you.
Have a nice day!
B.R,
Weidong