imx7 qmake 5.6.2 does not work (its look x86)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

imx7 qmake 5.6.2 does not work (its look x86)

1,902 次查看
atakanakbulut
Contributor II

Hello everyone , I am working on imx7 and i created my distro its working on board . I created qt toolchain but it is not working . toolchain qmake version 5.6.2 and i get this error.

(.qtversion[qt_version_tag]+0x0):-1: error: undefined reference to `qt_version_tag'  

my gcc path 

/opt/fsl-imx-x11/4.1.15-2.0.0/sysroots/x86_64-pokysdk-linux/usr/bin/arm-poky-linux-gnueabi/arm-poky-linux-gnueabi-gcc

my g++ path 

/opt/fsl-imx-x11/4.1.15-2.0.0/sysroots/x86_64-pokysdk-linux/usr/bin/arm-poky-linux-gnueabi/arm-poky-linux-gnueabi-g++

my qmake is auto-detected 5.6.2 

Also i have old release when i compilar old qmake i did not any problem .(qmake version 5.5.1)

 1.png

i am source needed parameters but doesnt work . Added qt defines but qmake looking for x86. When i added 

DEFINES += QT_NO_VERSION_TAGGING

in pro file problem is fixed but binay not running because of its looks x86 compilar . when i get binary info its 

ELF 64-bit LSB executable, x86-64, version 1 (GNU/Linux), dynamically linked, interpreter /lib64/ld-linux-x86-64.so.2, for GNU/Linux 2.6.32, BuildID[sha1]=6be4f7ebc9ef695084f1e117053ffc047b967f86, not stripped

my distro info 

For imx7 sabre board

$ MACHINE=imx7dsabresd source fsl-setup-release.sh -b build-x11 -e x11

Build release

$ bitbake fsl-image-qt5

Create toolchain


$ bitbake meta-toolchain-qt5

标签 (4)
0 项奖励
回复
2 回复数

1,484 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport
0 项奖励
回复

1,484 次查看
atakanakbulut
Contributor II

doesnt work for me. 

release 4.1.15-2.0.0 qmake is fail.  

i am triying freescale rocko yocto bsp but its not have meta-toolchain-qt when i i added manual i get error. 

atakan@atakan-argew1:~$ qmake --version
QMake version 3.0
Using Qt version 5.5.1 in /usr/lib/x86_64-linux-gnu

atakan@atakan-argew1:~$ /opt/fsl-imx-x11/4.1.15-2.0.0/sysroots/x86_64-pokysdk-linux/usr/bin/qt5/qmake --version
QMake version 3.0
Using Qt version 5.6.2 in /opt/fsl-imx-x11/4.1.15-2.0.0/sysroots/cortexa7hf-neon-poky-linux-gnueabi/usr/lib

0 项奖励
回复